2022-03-14 9:57 PM
Hi,
I am trying to initialize FDCAN for my project.
After the initialization I am clearing INIT bit in CCCR Register. The output what I can see is only CCE bit gets cleared but INIT bit is stuck at 1.
Below is my code snippet.
void Can_driver_init (void)
{
uint32_t StartAddress_l_u32 = CAN_RAM_OFFSET_CFG;
uint32_t RAMcounter_l_u32 = 0;
uint32_t ElementSize_l_u32 = (CAN_DATA_BYTES_CFG/4);
// Enable the peripheral clock for FDCAN
RCC->APB1HENR |= RCC_APB1HENR_FDCANEN;
// Exit from Sleep mode */
CAN->CCCR &= ~FDCAN_CCCR_CSR;
// Wait till the CSR bit is set in CCCR */
while (CAN->CCCR == FDCAN_CCCR_CSR); // Wait timeout to be added
// Request initialization */
CAN->CCCR |= FDCAN_CCCR_INIT;
// Wait until the INIT bit in CCCR register is set */
while ((CAN->CCCR & FDCAN_CCCR_INIT) != FDCAN_CCCR_INIT); // Wait timeout to be added
// Enable configuration change */
CAN->CCCR |= FDCAN_CCCR_CCE;
// Enable automatic retransmission */
CAN->CCCR &= ~FDCAN_CCCR_DAR;
// Disable transmit pause */
CAN->CCCR &= ~FDCAN_CCCR_TXP;
// Disable Protocol Exception Handling */
CAN->CCCR &= ~FDCAN_CCCR_PXHD;
// Set CAN Frame Format as CLASSIC*/
CAN->CCCR |= CAN_FRAME_CFG;
// Configure CAN Operation Mode as normal */
CAN->CCCR |= CAN_MODE_CFG;
// Set the nominal bit timing register for CAN Bit-rate*/
CAN->NBTP = (NBTP_NSJW_VAL_CFG << FDCAN_NBTP_NSJW_Pos) |
(NBTP_NTSEG1_VAL_CFG << FDCAN_NBTP_NTSEG1_Pos) |
(NBTP_NTSEG2_VAL_CFG << FDCAN_NBTP_NTSEG2_Pos) |
(NBTP_NBRP_VAL_CFG << FDCAN_NBTP_NBRP_Pos);
// Configure number of dedicated transmit buffers. */
CAN->TXBC = (NBR_OF_TXBUFFER_CFG << FDCAN_TXBC_NDTB_Pos);
// Configure Tx buffer element size */
CAN->TXESC |= (ElementSize_l_u32 << FDCAN_TXESC_TBDS_Pos);//TBD
// Configure Rx buffer element size */
CAN->RXESC |= (ElementSize_l_u32 << FDCAN_RXESC_RBDS_Pos);
//--------------------------------------------------------------------
//--------------------------------------------------------------------
// Message RAM configuration:
// ***************************
// ________
// 0x00 |________| Standard_filter[0]
// |________|
// |________|
// |||||||||| Rx_buffer[0]
// ||||||||||
// |||||||||| Rx_buffer[n]
// |________| Tx_buffer[0]
// |________|
// |________| Tx_buffer[n]
// ||||||||||
// ||||||||||
// |||||||||| FreeSpace
// ||||||||||
// ||||||||||
// @2560 ||||||||||
// Calculate each RAM block address
// -------------------------------
// Block 0: Standard Filters
// -------------------------------
// Standard filter list start address
CAN->SIDFC |= (StartAddress_l_u32 << FDCAN_SIDFC_FLSSA_Pos);
// Number of standard filter elements
CAN->SIDFC |= (NBR_OF_STD_FILTERS << FDCAN_SIDFC_LSS_Pos);
StartAddress_l_u32 += NBR_OF_STD_FILTERS;
// -------------------------------
// Block 1: Dedicated Rx Buffers
// -------------------------------
// Rx buffer list start address */
CAN->RXBC |= (StartAddress_l_u32 << FDCAN_RXBC_RBSA_Pos);
StartAddress_l_u32 += (NBR_OF_RXBUFFER_CFG * CAN_DATA_BYTES_CFG);
// Note: No register field is defined for declaring
// number of dedicated Rx buffers in STM32H7
// -------------------------------
// Block 2: Dedicated Tx Buffers
// --------------------------------
// Tx buffer list start address */
CAN->TXBC |= (StartAddress_l_u32 <<FDCAN_TXBC_TBSA_Pos);
// Number of dedicated Tx buffers */
CAN->TXBC |= (NBR_OF_TXBUFFER_CFG << FDCAN_TXBC_NDTB_Pos);
//--------------------------------
//--------------------------------
// Store the Addresses of different fields of CAN Message RAM
MsgRam.StandardFilterSA = SRAMCAN_BASE;
MsgRam.RxBufferSA = MsgRam.StandardFilterSA + (NBR_OF_STD_FILTERS * 4);
MsgRam.TxBufferSA = MsgRam.RxBufferSA + (NBR_OF_RXBUFFER_CFG * (CAN_DATA_BYTES_CFG * 4));
MsgRam.EndAddress = MsgRam.TxBufferSA + (NBR_OF_TXBUFFER_CFG * (CAN_DATA_BYTES_CFG * 4));
// Flush the allocated Message RAM area
for (RAMcounter_l_u32 = MsgRam.StandardFilterSA; RAMcounter_l_u32 < MsgRam.EndAddress; RAMcounter_l_u32 += 4U)
{
*(uint32_t *)(RAMcounter_l_u32) = 0x00000000;
}
/*--------------------------------------------------------------------
*--------------------------------------------------------------------*/
// Configure filter elements
CanIf_filterInit();
// Enable the interrupts
Can_driver_enableInterrupts();
// Request leave initialization
CAN->CCCR &= ~FDCAN_CCCR_INIT;
}
2023-01-19 1:18 PM
I am having the same issue with the INIT bit not clearing - did this get resolved?
2023-02-20 5:01 AM
Hi,
Any updates?
I am having the same issue but on STM32G431KBT6. I am using arm non eabi toolchain, assembly and cmsis copied from cube project + cmake.
I observed that the ARA bit is set just after enabling fdcan in rcc. The code to reproduce the issue:
RCC->APB1ENR1 |= RCC_APB1ENR1_FDCANEN;
FDCAN1->CCCR |= FDCAN_CCCR_INIT;
//here the ARA bit =1
while ((FDCAN1->CCCR & FDCAN_CCCR_INIT) != FDCAN_CCCR_INIT);
That happens only when using cmake to build target. I created a new empty project in STM32 cube IDE and added mentioned lines:
void main()
{
RCC->APB1ENR1 |= RCC_APB1ENR1_FDCANEN;
FDCAN1->CCCR |= FDCAN_CCCR_INIT;
//here the ARA bit =1
while ((FDCAN1->CCCR & FDCAN_CCCR_INIT) != FDCAN_CCCR_INIT);
}
The issue did not occur. I must not be doing something that STM32 Cube IDE is. I spent a lot of time trying to debug this issue...
Any ideas?
I found that somebody have the same issue:
STM32H743 FDCAN stuck in init mode - General Discussion - PlatformIO Community
2023-07-26 12:47 AM
Hello community
A little up for this subject because I have the same problem...
Does someone has any idea?
2024-07-25 7:18 AM
Same issue with STM32H7S7L8H6H