2023-01-11 12:03 AM
Hello,
I'm trying to setup interrupts using the user push button (B1) on the Nucleo-F429ZI board. The push button is connected to the microcontroller through the I/O line PC13.
What I did is that I mapped the PC13 to the GPIO_EXTI15 in STM32CubeMX and enabled the NVIC interrupt for EXTI15_10. Then I regenerated the code which gave me the following function in main:
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
/*Configure GPIO pin : PC13 */
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
}
I call it in the main after initializing the clocks. However, after the function has been executed, pressing the button does not trigger an interrupt. I enabled interrupt tracing and I can see that the interrupt is never triggered and my callback is therefor never called.
Did I do something wrong ? Thank you.
Solved! Go to Solution.
2023-01-12 12:40 AM
Yes they're enaled. HAL_Delay(10) is working and to be sure I use the __enable_irq() function.
2023-01-12 12:48 AM
Did you try with other interrupts ? not with the push button but with another pin that you can set and reset
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-12 5:16 AM
I finally found the problem... All the configuration was good, the only thing that broke my system was a preprocessor symbol define that was included in my example project : CMSIS_NVIC_VIRTUAL HSE_VALUE=8000000. I still don't know what purpose it serves.
In addition, the cmsis_nvic_virtual.h was used and some NVIC functions were redefined:
#define NVIC_SetPriorityGrouping __NVIC_SetPriorityGrouping
#define NVIC_GetPriorityGrouping __NVIC_GetPriorityGrouping
#define NVIC_EnableIRQ(IRQn) svcNVIC_func(2U, IRQn)
#define NVIC_GetEnableIRQ __NVIC_GetEnableIRQ
#define NVIC_DisableIRQ(IRQn) svcNVIC_func(4U, IRQn)
#define NVIC_GetPendingIRQ __NVIC_GetPendingIRQ
#define NVIC_SetPendingIRQ __NVIC_SetPendingIRQ
#define NVIC_ClearPendingIRQ(IRQn) svcNVIC_func(7U, IRQn)
#define NVIC_GetActive __NVIC_GetActive
#define NVIC_SetPriority __NVIC_SetPriority
#define NVIC_GetPriority __NVIC_GetPriority
#define NVIC_SystemReset __NVIC_SystemReset
Upon removing these two modifications, the button interrupt is now working correctly.
Thank you all for your help.