2014-08-15 9:56 AM
Dear friends. Show me please my mistake. When I debug the following program I even cannot get to ISR... I stay in infinite loop...
Thanks! void EXTI0_IRQHandler (void); int main(void) { /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup files (startup_stm32f429_439xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f4xx.c file */ /* Add your application code here */ /* Infinite loop */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); //Clck to GPIOG RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0); GPIO_InitTypeDef PortG_init, PortA_init; PortG_init.GPIO_Mode = GPIO_Mode_OUT; PortG_init.GPIO_OType = GPIO_OType_PP; PortG_init.GPIO_Pin = GPIO_Pin_13; PortG_init.GPIO_PuPd = GPIO_PuPd_NOPULL; PortG_init.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOG, &PortG_init); PortA_init.GPIO_Mode = GPIO_Mode_IN; PortA_init.GPIO_OType = GPIO_OType_PP; PortA_init.GPIO_Pin = GPIO_Pin_0; PortA_init.GPIO_PuPd = GPIO_PuPd_NOPULL; PortA_init.GPIO_Speed = GPIO_Low_Speed; GPIO_Init(GPIOA, &PortA_init); //GPIOA_Pin_0 as input EXTI_InitTypeDef PortA_Pin0; PortA_Pin0.EXTI_Line = EXTI_Line0; PortA_Pin0.EXTI_Mode = EXTI_Mode_Interrupt; PortA_Pin0.EXTI_Trigger = EXTI_Trigger_Rising; PortA_Pin0.EXTI_LineCmd = ENABLE; EXTI_Init(&PortA_Pin0); NVIC_InitTypeDef NVIC_PortA; NVIC_PortA.NVIC_IRQChannel = EXTI0_IRQn; NVIC_PortA.NVIC_IRQChannelPreemptionPriority = 0x01; NVIC_PortA.NVIC_IRQChannelSubPriority = 0x01; NVIC_PortA.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_PortA); while (1) { } } void EXTI0_IRQHandler (void) { GPIO_ToggleBits(GPIOG, GPIO_Pin_13); // delay(1000000); EXTI_ClearITPendingBit(EXTI_Line0); } Interesting thing...I'm working in IAR. When I was debugging watching locals in this part: PortA_Pin0.EXTI_Line = EXTI_Line0; PortA_Pin0.EXTI_Mode = EXTI_Mode_Interrupt; PortA_Pin0.EXTI_Trigger = EXTI_Trigger_Rising; PortA_Pin0.EXTI_LineCmd = ENABLE; EXTI_Init(&PortA_Pin0); PortA_Pin0.EXTI_LineCmd = ENABLE stayed DISABLED until I didn't changed compiler optimization from high to medium.... What didn't I take into account? Watching for other bugs....2014-08-16 8:40 PM
C++, or you're not actually generating an interrupt?
Does the pin have/need a pull up/down? Are you looking at the right edge? Can you print the state of the pin, via GPIO, in the while(1) loop?2014-08-17 9:14 AM
It was some sort of compiler behavior. When I checked low optimization compilation - everything started to work... One of the following steps is to understand the optimization.
''Can you print the state of the pin, via GPIO, in the while(1) loop?'' I saw the change in the IDR register - and that was very confusing. Thanks for the support, Clive1.2014-08-18 9:37 PM
You really should test/qualify your interrupt source, but your issue here probably is the race condition in the NVIC/EXTI. You should clear the interrupt early, not as the last thing.
void EXTI0_IRQHandler (void)
{
EXTI_ClearITPendingBit(EXTI_Line0); // Do this first to stop reentry, ideally you'd qualify the source
GPIO_ToggleBits(GPIOG, GPIO_Pin_13); // before toggling
}