2019-05-12 8:29 AM
Hello,
I hope someone can help with this riddle.
We just started working with our custom board, based on stm32h743 (untill now we worked with eval stm32h743-eval board).
The internal memories, GPIOs and other interfaces works OK, but we have the following strange issue with the external sram:
In our test we write 0x400 bytes (0x200 16-bytes words) and read these 0x400 bytes and compare values.
SRAM_Timing.AddressSetupTime = 0;
SRAM_Timing.AddressHoldTime = 1;
SRAM_Timing.DataSetupTime = 1;
SRAM_Timing.BusTurnAroundDuration = 0;
SRAM_Timing.CLKDivision = 16;
SRAM_Timing.DataLatency = 17;
SRAM_Timing.AccessMode = FMC_ACCESS_MODE_A;
g_hsram.Init.NSBank = FMC_NORSRAM_BANK3;
g_hsram.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
g_hsram.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;
g_hsram.Init.MemoryDataWidth = SRAM_MEMORY_WIDTH;
g_hsram.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
g_hsram.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
g_hsram.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
g_hsram.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
g_hsram.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
g_hsram.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
g_hsram.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
g_hsram.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
g_hsram.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;It "feels" as if some code action interrupt the sram conmtroller timing. Does it make sense ?
Thank you for any idea,
ran
Solved! Go to Solution.
2019-05-12 9:03 AM
Sounds more like the data never actually gets written, and you just see the data in the caches, until it gets replaced.
2019-05-12 9:03 AM
Sounds more like the data never actually gets written, and you just see the data in the caches, until it gets replaced.
2019-05-12 10:11 PM
I also suspected this, but I have configured 0x68000000 as non-cacheable in MPU.
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0x68000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_64MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
Is something wrong with this configuration ?
Thank you
2019-05-13 3:25 AM
Right!
I now see that it gives 0xfffffff in all reads.
What does it mean ?
2019-05-14 5:04 AM
Solved. BLE BLH pins were missing. Thx