2024-10-18 2:18 AM
In application we are using MCU part no STM32G0KCIU6 of LQFP32 / UFQFPN32 - GP package, can external oscillator of frequency 16MHz (Example: Part no ASEMB-16.000MHZ-LY-T) can be connected to pin no 2 which is dedicated for LSE clock frequency 32KHz. As per datasheet Pin assignment and description list Pin No 2 of MCU has additional options to configure as OSC_IN whether this pin can be configured for HSE requirement? Can external oscillator of frequency 16MHz can be connected to this Pin?
Solved! Go to Solution.
2024-10-18 3:56 AM
external Crystal oscillator have two pins OSC_IN and OSC_OUT as mentioned OSC_IN will be connected to PC14. suggest which pin can i connect OSC_OUT
2024-10-18 4:03 AM - edited 2024-10-18 4:09 AM
With Crystal oscillator you need to use only OSC_IN and in this package only OSC_IN is available:
So you need to use a Crystal oscillator not a Crystal/resonator.
Example: https://sourcewell.in/product/crystal-oscillators/
Hope it does answer your question.
2024-10-18 4:07 AM
@Welcome_123 wrote:suggest which pin can i connect OSC_OUT
When you're using an external oscillator, you bypass the STM32's internal oscillator.
The OSC_OUT or OSC32_OUT pin then becomes available as GPIO
See the Reference Manual:
2024-10-18 4:14 AM
can ST suggest 48MHz Crystal oscillator for this application
2024-10-18 4:23 AM - edited 2024-10-18 4:24 AM
@Welcome_123 wrote:
can ST suggest 48MHz Crystal oscillator for this application
You need a crystal oscillator powered with VDD of your MCU.
2024-10-18 4:26 AM
yes need a crystal oscillator powered with 3.3V
2024-10-18 5:05 AM
You suggested one in your opening post?
2024-10-18 5:45 AM
According to its datasheet: