cancel
Showing results for 
Search instead for 
Did you mean: 

External memories and FMC

GGran.2
Associate III

Hello,

in order to use external memories, is it mandatory to use the FMC?

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @GGran.2 ,

That depends on the memory you need to interface.

There are other external memory interfaces such as QuadsPI, OCTOSPI, XSPI etc .. even I2C and SPI could be an interface for some memories...

You need to provide more details about the device you need to manage with STM32.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

4 REPLIES 4
SofLit
ST Employee

Hello @GGran.2 ,

That depends on the memory you need to interface.

There are other external memory interfaces such as QuadsPI, OCTOSPI, XSPI etc .. even I2C and SPI could be an interface for some memories...

You need to provide more details about the device you need to manage with STM32.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thank you for the answer. My question was born following an answer to another my question in this forum concerning the speculation. In that answer a user wrote that the speculation on FMC is not useful while the speculation on external memories can be useful. Then I thought that the external memories can be acceded with different controllers and protocols.

FMC can be accessed the same way as internal memories taking into account some specificities: default MPU config, timings etc ..

Hope I answerd your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
prayerbalk
Associate

Hy GGran.2,

That depends on the memory you need to interface.