‎2020-04-15 02:41 AM
Hello,
this is my first project with stm mcu and my development board is on the way. I would like to make a hobby wav player and I have found a rather good recipe to start with - AN3126 Application note "Audio and waveform generation using the DAC in STM32 microcontrollers"
But I wonder where can I find the example code? I'll appreciate any hint about it.
Best Regards,
Anton
‎2020-04-15 08:05 AM
Hello
You can use the STM32CubeMX's sample examples, which are in the bellow directiory:
C:\Users\(Windows User Name)\STM32Cube\Repository\STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Examples
‎2020-04-15 08:24 AM
Or the H7, board specific ones
STM32Cube_FW_H7_V1.7.0\Projects\STM32H747I-DISCO\Examples
You'd nee to port over a DAC example
STM32Cube_FW_H7_V1.7.0\Projects\STM32H747I-EVAL\Examples\DAC\DAC_SignalsGeneration
‎2020-04-15 08:31 AM
:ok_hand:
‎2020-04-16 01:12 AM
Thank you @A_R​ amd @Community member​. I guess this means I should install STM32CubeMX but it shouldn't be a big problem to find it on the web site.