2011-02-12 12:39 PM
Hey,
I just spent a bunch of time sorting out how to get the darn PWM output on the blue LED on the STM32-Discovery board. After a lot of time pouring over the datasheets and forum posts I was finally able to work out the following code. Seems to work very well. RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE ); RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM3, ENABLE ); // Set the Vector Table base address at 0x08000000. NVIC_SetVectorTable( NVIC_VectTab_FLASH, 0x0 ); NVIC_PriorityGroupConfig( NVIC_PriorityGroup_4 ); // Configure HCLK clock as SysTick clock source. SysTick_CLKSourceConfig( SysTick_CLKSource_HCLK ); // Setup Blue LED on STM32-Discovery Board to use PWM. GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; // Alt Function - Push Pull GPIO_Init( GPIOC, &GPIO_InitStructure ); GPIO_PinRemapConfig( GPIO_FullRemap_TIM3, ENABLE ); // Map TIM3_CH3 to GPIOC.Pin8 // Let PWM frequency equal 100Hz. // Let period equal 1000. Therefore, timer runs from zero to 1000. Gives 0.1Hz resolution. // Solving for prescaler gives 240. TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct; TIM_TimeBaseStructInit( &TIM_TimeBaseInitStruct ); TIM_TimeBaseInitStruct.TIM_ClockDivision = TIM_CKD_DIV4; TIM_TimeBaseInitStruct.TIM_Period = 1000; TIM_TimeBaseInitStruct.TIM_Prescaler = 240; TIM_TimeBaseInit( TIM3, &TIM_TimeBaseInitStruct ); TIM_OCInitTypeDef TIM_OCInitStruct; TIM_OCStructInit( &TIM_OCInitStruct ); TIM_OCInitStruct.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1; // Initial duty cycle equals 0%. Value can range from zero to 1000. TIM_OCInitStruct.TIM_Pulse = 0; TIM_OC3Init( TIM3, &TIM_OCInitStruct ); TIM_Cmd( TIM3, ENABLE ); Also, below is a useful macro that sets the PWM duty cycle once the output is running. // Set duty cycle when using TIM3 as a PWM output. &sharpdefine SetTIM3Duty( val ) TIM3->CCR3 = val It's neat to see the blue LED ramping and fading smoothly. #stm32 #pwm #pwm #discovery #stm32f100rb #output2014-06-03 4:12 AM
Any ideas why this is happening?
Yes, randomly declaring variables in the middle of a subroutine is a C++ syntax, for real C the variable definitions need to be made at the opening scope (ie '{') before any code statements. If your code was in MAIN.CPP your compiler might tolerate it.2014-06-03 4:49 AM
Hi
'' #268: declaration may not appear after executable statement in block '' means you cannot declare variables after code, variables must be declared at the start of a function block. ''//TIM 3 Config
void Timer_Configuration_Sec(void) {GPIO_InitTypeDef GPIO_InitStructure;
// Setup LED as PWM output GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init( GPIOC, &GPIO_InitStructure ); GPIO_PinRemapConfig( GPIO_FullRemap_TIM3, ENABLE ); //LED connected to Pin 6, Port CTIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct; TIM_TimeBaseInitStruct.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInitStruct.TIM_Period = Timer_Period_Value; TIM_TimeBaseInitStruct.TIM_ClockDivision = TIM_CKD_DIV1; //TIM_TimeBaseInitStruct.TIM_RepetitionCounter = 0; TIM_TimeBaseInitStruct.TIM_Prescaler = Timer_Prescaler_Value_Sec; TIM_TimeBaseInit(Timer_Used_Sec,&TIM_TimeBaseInitStruct); TIM_OCInitTypeDef TIM_OCInitStruct; TIM_OCStructInit( &TIM_OCInitStruct ); TIM_OCInitStruct.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1; // Initial duty cycle equals 0%. Value can range from zero to 1000. TIM_OCInitStruct.TIM_Pulse = SetTIM3Duty(0); TIM_OC3Init( TIM3, &TIM_OCInitStruct ); // Initialize Timer Channel 3 setup TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable); // TIM_ClearITPendingBit(Timer_Used_Sec,TIM_IT_Update); // TIM_ITConfig(Timer_Used_Sec,TIM_IT_Update,ENABLE); // TIM_Cmd(Timer_Used_Sec,ENABLE); }'' I have highlighted the offending lines. Strange the compiler picked up on he 2nd instance?!?
2015-03-18 11:27 AM
When i run this code I keep getting errors like these;
linking....\ro6.axf: Error: L6218E: Undefined symbol GPIO_Init (referred from main.o)..\ro6.axf: Error: L6218E: Undefined symbol GPIO_PinAFConfig (referred from main.o)..\ro6.axf: Error: L6218E: Undefined symbol RCC_AHBPeriphClockCmd (referred from main.o)..\ro6.axf: Error: L6218E: Undefined symbol RCC_APB1PeriphClockCmd (referred from main.o).I'm new enough to using the board so could be a small thing. Any ideas what I'm doing wrong?2015-03-18 11:46 AM
You'd need to add the stm32xxx_rcc.c and stm32xxx_gpio.c files into your project.
/public/STe2ecommunities/mcu/Lists/STM32Discovery/Attachments/13561/keil_stm32l_proj.jpg
________________ Attachments : keil_stm32l_proj.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzsG&d=%2Fa%2F0X0000000bSP%2FmFOdz0aHKjmXlFuIbE9eYkjEOVZo7aPVgeUqIZ9l474&asPdf=false2015-03-18 11:59 AM
Clive,
I already have those files in my project folder and have the pathway to the folder containing all the files chosen.2015-03-18 12:13 PM
I already have those files in my project folder and have the pathway to the folder containing all the files chosen.
ZIP/RAR the project tree, I'll rack it up here and see. The error messages suggest it's not pulling that stuff in.
The other meta-data in the project are the preprocessor defines ''USE_STDPERIPH_DRIVER, STM32L1XX_HD, USE_STM32L152D_EVAL''
2015-03-20 3:23 AM
Thats my project that I have been trying to get working.
________________ Attachments : ro4.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzzH&d=%2Fa%2F0X0000000bSM%2Fi9yOef9NeC0erU.HOd.o96yCuxyE1Majaa9o7TBjynU&asPdf=false2015-03-20 1:31 PM
Ok, that's just the project definition file, not the project. Doesn't look like you have the defines set.
2015-12-13 8:24 AM
Hello,
I tried get PWM output on pin PA After lot of time I still can't do it. Can you help me please? Here is the code: Comented parts works on PC7, so I tried changed values.//RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO, ENABLE );
//RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM3, ENABLE );
RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE );
RCC_APB2PeriphClockCmd( RCC_APB2Periph_TIM1, ENABLE );
GPIO_StructInit(&GPIO_InitStructure);
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
//GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;
//GPIO_Init( GPIOC, &GPIO_InitStructure );
//GPIO_PinRemapConfig( GPIO_FullRemap_TIM3, ENABLE );
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_Init( GPIOA, &GPIO_InitStructure );
TIM_TimeBaseStructInit( &TIM_TimeBaseInitStruct );
TIM_TimeBaseInitStruct.TIM_Prescaler = 24-1;
TIM_TimeBaseInitStruct.TIM_Period = 20000 - 1;
TIM_OCStructInit( &TIM_OCInitStruct );
TIM_OCInitStruct.TIM_OutputState = TIM_OutputState_Enable;
//TIM_TimeBaseInit( TIM3, &TIM_TimeBaseInitStruct );
//TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1;
//TIM_OC2Init( TIM3, &TIM_OCInitStruct );
//TIM_Cmd( TIM3, ENABLE );
TIM_TimeBaseInit( TIM1, &TIM_TimeBaseInitStruct );
TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OC3Init( TIM1, &TIM_OCInitStruct );
TIM_Cmd( TIM1, ENABLE );
//TIM3->CCR2 = 1000;
TIM1->CCR3 = 1000;
2015-12-13 11:06 AM
/* Main Output Enable, and Input */
TIM_CtrlPWMOutputs(TIM1, ENABLE);