cancel
Showing results for 
Search instead for 
Did you mean: 

Example code to use with STM32Cube

hchaudhary
Associate
Posted on July 02, 2014 at 21:00

Hi All, I am new to the STM32 MCU.

I am trying implement code for USART receive in interrupt mode using the HAL generated by STM32CubeF4. Are there any example codes that I can study?

Thanks

MCU: STM32F4

IDE: KEIL MKD 4.73 Pro

#stmcube-stm32f4-usart
1 REPLY 1
Amel NASRI
ST Employee
Posted on July 03, 2014 at 11:58

Hi,

You can refer to the various examples in the Cube package (

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF259243

).

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.