2024-06-25 10:56 PM
Hi, I have a problem. when I used old cube ide version, ı can changing physical address and ethernet module is to take ip address. But when I use new version I want to edit phy address but this area is not in new version.
That's why I can't use the Ethernet module in the new version.
Can you help me on how to use the Lan8720 Ethernet module in the new version?
2024-06-25 10:57 PM
Old Version Stm32Cubeide
New Version Stm32cubeide
2024-06-25 11:32 PM
For now, I updated the value of this constant to 0x1 and the module was able to get the IP address. However, when I generate my code with different changes, I need to change the constant again.
2025-03-23 7:04 PM
Did you ever find a solution to this? I am having the same problem. Thanks
2025-03-24 12:32 AM
I couldn't find any solution other than the one in the screenshot above