2013-05-19 1:04 AM
Quote from Reference Manual
Bits 7:6 PCF: Pass control frames
These bits control the forwarding of all control frames (including unicast and multicastPAUSE frames). Note that the processing of PAUSE control frames depends only on RFCEin Flow Control Register[2].00: MAC prevents all control frames from reaching the application01: MAC forwards all control frames to application except Pause control frames
10: MAC forwards all control frames to application even if they fail the address filter11: MAC forwards control frames that pass the address filter.These bits control the forwarding of all control frames (including unicast and multicastPAUSE frames). Note that the processing of PAUSE control frames depends only on RFCEin Flow Control Register[2].00 or 01: MAC prevents all control frames from reaching the application
10: MAC forwards all control frames to application even if they fail the address filter11: MAC forwards control frames that pass the address filter.Looks like someone tried to fix manual and left old text.So what is correct for PCF=01 ?2013-06-05 8:50 AM
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-09-07 3:20 AM
So when can we expect to get updated Reference Manual?