cancel
Showing results for 
Search instead for 
Did you mean: 

Error while sending data on UART continuously

SARTHAK KELAPURE
Associate II
Posted on December 19, 2017 at 06:43

I am interfacing ESP8266 with my Murata LoRa board(though not using LoRa), so let us just say I am using STM32L072CZ with ESP8266 connected on UART1(Pin9,10). I am seeing a strange behavior from STM UART.

The code being used is as below,

//HEADERS

char cmd[]='AT+CWLAP\r\n';

...

int main()

{

//INIT

...

while(1)

{

HAL_UART_Transmit(&huart1,(uint8_t*)cmd,strlen(cmd),0xFFFF);

}

This works well for the first few iterations and then fails as seen in attachment. Please help and pin point the problem and solution.

#stm32l072 #stm32 #stm32l0-uart
5 REPLIES 5
Doug Kehn
Senior
Posted on December 19, 2017 at 14:26

What is the return value from HAL_UART_Transmit()?

Try setting a breakpoint when the error occurs to inspect registers, etc.

Andrew Neil
Evangelist III
Posted on December 19, 2017 at 18:21

char cmd[]='AT+CWLAP\r\n';

Note that you don't need the \n here.

It should be benign, but better to get rid of it and remove all doubt ...

Andrew Neil
Evangelist III
Posted on December 19, 2017 at 18:27

Please make use of the Syntax Highlighter to properly present source code:

while(1)
{
 HAL_UART_Transmit( &huart1, (uint8_t*)cmd, strlen(cmd), 0xFFFF );
}
�?�?�?�?�?�?�?�?�?

That is a great way to crash any AT Command interface!

You should never send another AT command before you have had the full response from the previous one!

Posted on December 19, 2017 at 18:39

I made the foolish mistake of using the Syntax Highlighter - so that post is now stuck in Moderation.

:(

Sending out commands in a tight 'while' loop is a sure way to crash

any

 

AT Command interface!

 You should

never

 

send another AT command before you have had the

full

 

response from the previous one!
Posted on December 20, 2017 at 08:57

Sending out commands in a tight 'while' loop is a sure way to crash

any

 

AT Command interface!

Nevertheless, a great idea for testing, should you ever write an AT command interface... 😉

Jan

PS. Just yesterday 've been bitten by the 'overflow when not cleared triggers Rx interrupt infinitely' gotcha of the STM32 USART...