cancel
Showing results for 
Search instead for 
Did you mean: 

Error mounting SD Card in 4-bit mode in stm32f756zg

dharanik_1399
Associate II

Hi,

 

I am encountering an issue with mounting the SD card in 4-bit mode on my STM32F756ZG microcontroller. Despite using the BSP driver (bsp_driver_sd), the SD card fails to initialize and mount correctly, resulting in an initialization error and the FR_NOT_READY_ERROR status.

Thanks&Regards

2 REPLIES 2
mÆŽALLEm
ST Employee

Hello,

See this thread

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
bramble
Senior

Hi @dharanik_1399 , I ran into the same problem very recently (on STM32H755). There could be several reasons for the problem you report but I suggest that you check this: https://community.st.com/t5/stm32-mcus-embedded-software/sdcard-with-sdmmc-on-stm32h755zi-nucleo/td-p/770582 .