Skip to main content
Senior
February 4, 2025
Solved

STM32H563VIT6 DAC1 Output Unexpected

Driving DAC1 channel 1 with

 

 

 

 

HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
...
while (1) {
 HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 4095UL);
 HAL_Delay(100UL);
 HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 0UL);
 HAL_Delay(100UL);
}

 

 

 

 

to generate 5 Hz, 50% duty cycle, 0 - 2.5v. Amplitude as expected but frequency varies from 1 - 4s and duty cycle varies from 20 - 80%: not expected. DAC1 configured like

mccabehm_1-1738710940044.png

DAC1 clocked at 65 MHz. When I step into HAL_DAC_SetValue() I see where the 0 - 4095 value is written to data register (12-bit, right-aligned). But sometimes after writing 4095 the output pin reads zero; and sometimes after writing zero the output pin reads 2.5v. I can't explain why this happens. DAC Instance following write looks like

mccabehm_2-1738711213554.png

I am the only writer on the data register.

This topic has been closed for replies.
mccabehmBest answer
Senior
February 8, 2025

9 replies

mccabehmAuthor
Senior
February 6, 2025

Custom board. I lifted the op amp pin connected to PA4 (DAC1 channel 1). Same behavior. This isolates the problem to the MCU and DAC peripheral.

mccabehmAuthor
Senior
February 6, 2025

Using same custom board, I ran an old project capable of generating the desired waveform. It works; desired waveform generated.

The new project (cannot generate desired waveform) used STM32CubeMX 6.13 and STM32Cube FW_H5 V1.4.0.

The old project (waveform good) used STM32CubeMX 6.12 and STM32Cube FW_H5 V1.3.0. I migrated the old project to STM32CubeMX 6.13 and STM32Cube FW_H5 V1.4.0. Now the old project which used to work -- fails. It manifests the same weird DAC behavior as the new project.

The code generated from the IOC file is identical. So the only difference is FW_H5 V1.4.0 vs FW_H5 V1.3.0.

How do I revert the project to STM32CubeMX 6.12 and FW_H5 V1.3.0?

waclawek.jan
Super User
February 6, 2025

What is the reference, VREF+?

JW

mccabehmAuthor
Senior
February 6, 2025

2.5v

waclawek.jan
Super User
February 6, 2025

Did you measure it?

JW

mccabehmAuthor
Senior
February 6, 2025

Yes. 2.57 to be exact. Stable.

mccabehmAuthor
Senior
February 7, 2025

I conclude: either the following code is wrong for running the DAC

 

HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
...
while (1) {
 HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 4095UL);
 HAL_Delay(100UL);
 HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 0UL);
 HAL_Delay(100UL);
}

 

or there's something wrong with migrating to STM32CubeMX 6.13 and STM32Cube FW_H5 V1.4.0 for H563.

If the migration is the problem, I need to revert a project from H5 V1.4.0 to V1.3.0. How to do that easily? Or do I remove H5 V1.4.0 from the repository and then re-create a project to grab the latest firmware version?

mccabehmAuthor
Senior
February 7, 2025

Comparing stm32h5xx_hal_msp.c from the "good" project and the "bad" project I see the "good" project has the following, which is absent from the "bad" project

 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(hdac->Instance==DAC1)
 {
 /* USER CODE BEGIN DAC1_MspInit 0 */

 /* USER CODE END DAC1_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DAC;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 Adding the above code to the "bad" project's stm32h5xx_hal_msp.c fixes the problem.

What needs to change in the "bad" project's IOC file to add the above code to stm32h5xx_hal_msp.c? There is nothing obvious in the GUI representations of the IOC files to explain the difference.

I am attaching IOC files from "good" and "bad" projects. I don't see anything in a diff of the 2 files to explain the missing code.

The stm32h5xx_hal_msp.c for the "good" project was generated with STM32CubeMX v6.12.0. The stm32h5xx_hal_msp.c for the "bad" project was generated with STM32CubeMX v6.13.0. At this point I am suspicious of MX 6.13.0.

mccabehmAuthorBest answer
Senior
February 8, 2025