2022-05-19 8:19 AM
Hello, I want to write/read on the flash memory. For that I made a small program (attached). My program works on Keil5 but when I switch to Atollic TrueStudio when I want to debug an error message tells me No source available for "__do_global_dtors_aux() at 0x80001ac". I can't seem to solve this problem, does anyone have any ideas? (I use an F401RE)
2022-05-20 2:49 AM
That sounds like a library function - so wouldn't be expected to have source?
If it worked on Keil, that will be using different libraries from Atollic - so are you sure you have this correctly set up for TrueStudio.
Note that the CubeIDE has replaced TrueStudio ...
2022-05-20 2:52 AM
"That sounds like a library function"
Indeed - A Google search for "__do_global_dtors_aux" finds this (amongst others):
https://stackoverflow.com/questions/6477494/do-global-dtors-aux-and-do-global-ctors-aux
Also note that this is for C++ - so is your project properly configured for C++ ?
2022-05-23 2:55 AM
Hi, thanks for your answer, I program in C. But I found an answer in the following link : Integrating STM32CubeProgrammer in Atollic TrueSTUDIO.
I now use STM32CubeProgrammer to load my program on the board and I debug with Atollic. The tutorial is very simple to follow and worked for me the first time.
2022-05-23 4:01 AM
Again, note that Atollic is now obsolete.
If the issue is now resolved, please mark the solution