cancel
Showing results for 
Search instead for 
Did you mean: 

Error initializing uart2 for STM32F072CBT6 processor

mhou
Associate II

We wanted to use the uart2 serial port of STM32F072CBT6. We used the STM32CUBE tool to generate the code, but the debugging found that we could not enter the interrupt of uart2.We had no problem setting uart1 and uart3 to use before.The initialization Settings of uart2 are as follows. Please help to check whether there is any problem. Thank you very much!

static void MX_DMA_Init(void) 
{
  /* DMA controller clock enable */
  __HAL_RCC_DMA1_CLK_ENABLE();
 
  /* DMA interrupt init */
  /* DMA1_Channel4_5_6_7_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Channel4_5_6_7_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Channel4_5_6_7_IRQn);
 
}
 
static void MX_USART2_UART_Init(void)
{
 
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 9600;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
 
}
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
 
  GPIO_InitTypeDef GPIO_InitStruct;
  if(huart->Instance==USART2)
  {
  /* USER CODE BEGIN USART2_MspInit 0 */
 
  /* USER CODE END USART2_MspInit 0 */
    /* Peripheral clock enable */
    __HAL_RCC_USART2_CLK_ENABLE();
  
    /**USART2 GPIO Configuration    
    PA2     ------> USART2_TX
    PA3     ------> USART2_RX 
    */
    GPIO_InitStruct.Pin = GPIO_PIN_2;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF1_USART2;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
    GPIO_InitStruct.Pin = GPIO_PIN_3;
    GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Alternate = GPIO_AF1_USART2;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
    /* USART2 DMA Init */
    /* USART2_RX Init */
    hdma_usart2_rx.Instance = DMA1_Channel5;
    hdma_usart2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_usart2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_usart2_rx.Init.MemInc = DMA_MINC_ENABLE;
    hdma_usart2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
    hdma_usart2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
    hdma_usart2_rx.Init.Mode = DMA_NORMAL;
    hdma_usart2_rx.Init.Priority = DMA_PRIORITY_LOW;
    if (HAL_DMA_Init(&hdma_usart2_rx) != HAL_OK)
    {
      _Error_Handler(__FILE__, __LINE__);
    }
 
    __HAL_LINKDMA(huart,hdmarx,hdma_usart2_rx);
 
    /* USART2_TX Init */
    hdma_usart2_tx.Instance = DMA1_Channel4;
    hdma_usart2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
    hdma_usart2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_usart2_tx.Init.MemInc = DMA_MINC_ENABLE;
    hdma_usart2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
    hdma_usart2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
    hdma_usart2_tx.Init.Mode = DMA_NORMAL;
    hdma_usart2_tx.Init.Priority = DMA_PRIORITY_LOW;
    if (HAL_DMA_Init(&hdma_usart2_tx) != HAL_OK)
    {
      _Error_Handler(__FILE__, __LINE__);
    }
 
    __HAL_LINKDMA(huart,hdmatx,hdma_usart2_tx);
 
    /* USART2 interrupt Init */
    HAL_NVIC_SetPriority(USART2_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(USART2_IRQn);
  /* USER CODE BEGIN USART2_MspInit 1 */
 
  /* USER CODE END USART2_MspInit 1 */
  }
 
}
 
void HAL_UART_MspDeInit(UART_HandleTypeDef* huart)
{
 
  if(huart->Instance==USART2)
  {
  /* USER CODE BEGIN USART2_MspDeInit 0 */
 
  /* USER CODE END USART2_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_USART2_CLK_DISABLE();
  
    /**USART2 GPIO Configuration    
    PA2     ------> USART2_TX
    PA3     ------> USART2_RX 
    */
    HAL_GPIO_DeInit(GPIOA, GPIO_PIN_2|GPIO_PIN_3);
 
    /* USART2 DMA DeInit */
    HAL_DMA_DeInit(huart->hdmarx);
    HAL_DMA_DeInit(huart->hdmatx);
 
    /* USART2 interrupt DeInit */
    HAL_NVIC_DisableIRQ(USART2_IRQn);
  /* USER CODE BEGIN USART2_MspDeInit 1 */
 
  /* USER CODE END USART2_MspDeInit 1 */
  }
 
}
 
void DMA1_Channel4_5_6_7_IRQHandler(void)
{
  /* USER CODE BEGIN DMA1_Channel4_5_6_7_IRQn 0 */
 
  /* USER CODE END DMA1_Channel4_5_6_7_IRQn 0 */
  HAL_DMA_IRQHandler(&hdma_usart2_tx);
  HAL_DMA_IRQHandler(&hdma_usart2_rx);
  /* USER CODE BEGIN DMA1_Channel4_5_6_7_IRQn 1 */
 
  /* USER CODE END DMA1_Channel4_5_6_7_IRQn 1 */
}
 
/**
* @brief This function handles USART2 global interrupt / USART2 wake-up interrupt through EXTI line 26.
*/
void USART2_IRQHandler(void)
{
  /* USER CODE BEGIN USART2_IRQn 0 */
 
  /* USER CODE END USART2_IRQn 0 */
  HAL_UART_IRQHandler(&huart2);
  /* USER CODE BEGIN USART2_IRQn 1 */
 
  /* USER CODE END USART2_IRQn 1 */
}

This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9

Does in end up in _Error_Handler()?

Does HAL_UART_MspInit() get called?

Afraid you're going to have to debug this on the system in question. Use the Peripheral view to check RCC, GPIO and USART2 register settings are correct/expected.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

hi Clive,

Thank you for your reply.

At present, the program can run normally without stopping in in _Error_Handler(), but it cannot enter the interrupt, which makes me confused.

And where is the code which would initiate an interrupt?

Do you transmit a message?

Make sure GPIOA clock is enabled.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mhou
Associate II
Yes, I passed the message through the serial port and enabled the serial port interrupt.
void SystemClock_Config(void)
{
 
  RCC_OscInitTypeDef RCC_OscInitStruct;
  RCC_ClkInitTypeDef RCC_ClkInitStruct;
  RCC_PeriphCLKInitTypeDef PeriphClkInit;
 
    /**Initializes the CPU, AHB and APB busses clocks 
    */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
  RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
 
    /**Initializes the CPU, AHB and APB busses clocks 
    */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
 
  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;
  PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
 
    /**Configure the Systick interrupt time 
    */
  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
 
    /**Configure the Systick 
    */
  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
  /* SysTick_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
 
static void MX_GPIO_Init(void)
{
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOF_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
 
}
 
void HAL_MspInit(void)
{
  /* USER CODE BEGIN MspInit 0 */
 
  /* USER CODE END MspInit 0 */
 
  __HAL_RCC_SYSCFG_CLK_ENABLE();
  __HAL_RCC_PWR_CLK_ENABLE();
 
  /* System interrupt init*/
  /* SVC_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(SVC_IRQn, 0, 0);
  /* PendSV_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(PendSV_IRQn, 0, 0);
  /* SysTick_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
 
  /* USER CODE BEGIN MspInit 1 */
 
  /* USER CODE END MspInit 1 */
}
 
 /* USART2 interrupt Init */
    HAL_NVIC_SetPriority(USART2_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(USART2_IRQn);

ZIP up a complete, compilable project, and attach as a single file, see paper clip icon, lower left below message edit box.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mhou
Associate II

hi Clive,

Attached is our test project, which we compiled using the IRA tool. Please receive it.Thanks again for your support!

mhou
Associate II

IAR tool;p

Your code doesn't do anything that would precipitate a USART2 interrupt.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mhou
Associate II

We have connected a device in uart2, which will continuously send data to STM32's uart2 through the serial port, and the program cannot enter the interrupt.Connect this device to uart1 and uart3 for normal access interruption.