cancel
Showing results for 
Search instead for 
Did you mean: 

Error in Writing External Flash STM32H750B-DK

ZExpo.1
Senior

ST-LINK SN : 002F00134D46501420383832

ST-LINK FW : V3J12M3

Board : STLINK-V3MINIE

Voltage : 3.43V

SWD freq : 8000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x450

Revision ID : Rev V

Device name : STM32H7xx

Flash size : 128 KBytes

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0x90

 

 

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a05624.srec

File : ST-LINK_GDB_server_a05624.srec

Size : 169.02 KB

Address : 0x08000000

 

 

Erasing memory corresponding to segment 0:

Erasing memory corresponding to segment 1:

Erasing external memory sectors [0 1]

Erasing memory corresponding to segment 2:

Erasing external memory sector 16

Download in Progress:

 

 

File download complete

Time elapsed during download operation: 00:00:10.115

 

 

 

Verifying ...

 

 

 

 

Error: Data mismatch found at address 0x90000003 (byte = 0x20 instead of 0x24)

 

 

Error: Download verification failed

 

 

Encountered Error when opening C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.0.202305091550\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

 

34 REPLIES 34

I have tried with different values and it seems to be working fine , But I tried to mass erase the NOR FLash and Got this Screenshot (30).pngI again wrote in the last memory address 0x97FE0000 and the data seems to be written perfectly fine as shownScreenshot (31).png

 

oh, it seems mass erase not fully functional. But as I remember, the more important is, to program code or data, the flow is erase block(s) + program block(s), random data files may be used to test if such operation is fully functional.

As shown in the pictures I can confirm that the data is not erased from the NOR Flash it can Only Be re written

Screenshot (36).pngScreenshot (37).png

Could You please share a External Flash loader which can only check single Nor Flash (We have 2 Separate Nor Flash on board)
RW187 (MT25QL512) x2

Sorry I don't have such kind of External Flash loader. All the External Flash loader files I have are from STM32CubeProgrammer installation.