2024-07-05 10:44 PM - edited 2024-07-06 11:11 PM
I am trying to upload the code to my target STM32F407 but below error is showing up. I tried some of suggestions but problem is still there. I am using Version: 1.15.1. Debug log file also attached.
1) Doing Mass Erase of flash,
2) Updating ST Link Firmware
3) Set Reset Behavior: None
4) Uncheck Enable Live Expressions
Update: I moved to STM32Cube programmer instead of using STM32cubeide, and able to upload the code after reducing ST-Link Frequency to 15Khz. Is it due to my target board poor design or something else. I am using Discovery Board ST-LINK to upload
Solved! Go to Solution.
2024-07-06 11:10 PM
Pls note issue has been solved. The problem was with jumper cables between ST-LINK and Target board. We used new cables and all in single ribbon, so now it is working fine.
I conclude EMI was issue..
2024-07-06 11:10 PM
Pls note issue has been solved. The problem was with jumper cables between ST-LINK and Target board. We used new cables and all in single ribbon, so now it is working fine.
I conclude EMI was issue..