Solved
Error in Final Launch Sequence
- 3 replies
- 5811 views
I am trying to upload the code to my target STM32F407 but below error is showing up. I tried some of suggestions but problem is still there. I am using Version: 1.15.1. Debug log file also attached.
1) Doing Mass Erase of flash,
2) Updating ST Link Firmware
3) Set Reset Behavior: None
4) Uncheck Enable Live Expressions

Update: I moved to STM32Cube programmer instead of using STM32cubeide, and able to upload the code after reducing ST-Link Frequency to 15Khz. Is it due to my target board poor design or something else. I am using Discovery Board ST-LINK to upload