2019-04-08 6:07 PM
in my h/w, i cannot control boot0 pin to high level for dfuse demo program.
however, i find that
When the entire flash memory is erased, st32L4 chip automatically goes to enter usb dfu mode.
hence,
i want to know how to erase the entire flash memory inside the main() function.
please let me know it is possible or not
thanks a lot
2019-04-08 8:22 PM
Review library code and reference manual
I would probably add code in Reset Handler, that copied itself to RAM and jump to it. The code would drive the flash peripheral registers to mass erase, then perform a software reset.