2007-10-22 03:31 AM
energy meter STM32F101xx
2011-05-17 03:16 AM
Hi Franco,
What is your battery voltage ; is it 3.0v or less /more ? You can refer to our Datasheet on web (rev3) it includes all what you need and also you can have a look on our Low power reference for your energy meter design with STM32 in this Application Note : ''STM32F101xx and STM32F103xx low-power modes''. Enjoy ;) Regards, STOne-322011-05-17 03:16 AM
He at All
Sorry for my continualy question The my application must be function in battery mode in this function what is the current used when the processor is in standby mode? is 2uA is correct? plus if the RCT is on is 1.4uA tot. the current is 3.4uA? The time from standby to a main function is 50us? Thanks Franco2011-05-17 03:16 AM
Hi obtronix,
150 and 200 µs are the Maximum timing in worst cases condition ( Hot /Cold temperatures, low/High VDD level from 2 to 3.6Volts. The typical value is of course less , for example only 50µs for Wake-up from standby mode + your reset firmware code & PLL lock time etc.... By the way, what is your application configuration and your expected life of Battery ? are you using other components such as a Glass LCD like on most of metering products. Regards, STOne-32 [ This message was edited by: STOne-32 on 21-10-2007 19:38 ]2011-05-17 03:16 AM
looking at the new datasheets the startup time is 150usec + 200 usec if you are using the PLL.
2011-05-17 03:16 AM
Quote:
On 21-10-2007 at 19:37, Anonymous wrote: Hi obtronix, By the way, what is your application configuration and your expected life of Battery ? are you using other components such as a Glass LCD like on most of metering products. Regards, STOne-32 I am using a glass LCD, which brings up a question, do you think the STM32 series will ever have a internal LCD driver like the MSP430/AVR/MaxQ chips have? Seem like a common thing required for power meters/glocose meters, which this processor is aimed at (according to ST's brochures). Takes a lot of area to add an external LCD driver chip. [ This message was edited by: obtronix on 23-10-2007 03:36 ]2011-05-17 03:16 AM
Thanks for your assistance
Franco