Posted on May 17, 2011 at 13:15Hi at all I this my application I must connected more ACS device (24 device) for command AC motor mini-motor electrovalve all in 230Vac 50hz. I can use the stm32f101 directed powered with trasfomless a 230Vac and drive...
Posted on May 17, 2011 at 12:22Hi at all I have one question, when the microcontroller is insert in the PCB at the first time, no program is load no clock is start, the micro is virgin, what is the current consumation at 3,3 volt? I have chk in this...
Posted on May 17, 2011 at 12:16He at All Sorry for my continualy question The my application must be function in battery mode in this function what is the current used when the processor is in standby mode? is 2uA is correct? plus if the RCT is on i...
Posted on May 17, 2011 at 12:16He at All I must conected the pin on STm32f101x6 and I have any question 1)what is the level in PIN BOOT0&1 in normal operation? 2)waht is the level on Boot0& Boot1 in up-date flash when use the Usrat1? 3)the all pin n...