2021-03-23 10:27 AM
The need I have is to count the encoder pulses on each front of the two channels (x4) always incrementing the counter independantly on the encoder direction and only have a tag on the direction changes.
I configured the TIM2 as encoder input (as shown in the picture TIM2 Config) with the counter preload to 1 and generate the TRGO to the TIM5 used as slave to count the encoder pulses.
The problem I have is that in the TIM5->CNT I have only half pulses as the counter x2 instead of x4.
Many thanks in advance to who will help me to solve this issue.
2021-03-23 1:48 PM
Connect the two lines physically to two timers' CH1 and CH2; use one timer to detect direction and in the other count edges for both channels and then add them together.
JW