cancel
Showing results for 
Search instead for 
Did you mean: 

Enable LTDC in CUBEMX

leddel32
Associate II

Hi,

We are in the designing phase of a STM32H7 board which will control a RGB24 display. To check which package would suit are needs the best we would like to see the RGB pinout on different MCU's. But for some reason I don't find the LTDC interface at the multimedia tab of these H7 controllers. 

If I open the boardfile of the H7 discovery board with display I do see the LTDC interface at the multimedia tab.

When we start a plain stm32H7S3L8HxH cubemx project. How to enable the LTDC interface?

Best regards

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Simply because STM32H7S3 doesn't have LCD-TFT interface which is not the case of STM32H7S7 (the one used on the DK board): 

From the datasheet:

SofLit_1-1735900526883.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

Simply because STM32H7S3 doesn't have LCD-TFT interface which is not the case of STM32H7S7 (the one used on the DK board): 

From the datasheet:

SofLit_1-1735900526883.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi Soflit,

 

Your absolutely right. My mistake.

Thank you.

 

Best regards,

 

 

Hello @leddel32 ,

Next time please accept the comment that answered your question and not your comment confirming the answer.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.