cancel
Showing results for 
Search instead for 
Did you mean: 

Emulating EEPROM when WWDG is running

Danish1
Lead III

I am trying to use FLASH to emulate EEPROM on stm32F767 based on AN3969. My FLASH is organised as a single bank, so executing from FLASH I would expect execution to stall while writing / erasing. The longest stall is when erasing a sector, which might take 0.5 s for a 32k sector at PSIZE=32 according to the data sheet.

However, with APB1 clocking at 36 MHz, I need to service the WWDG at least every 58 ms, so a stall of 0.5 s causes a WWDG reset, which is what I see.

I have tried placing the relevant routines in ITCM RAM but I still get the WWDG reset. I have disabled all interrupts, so my FLASH_WaitForLastOperation() polls the SysTick interrupt to increment its timeout counter. And similarly I tried to feed the WWDG in the event of a pending WWDG interrupt.

Does anyone know of any "gotchas" as to why I am still getting a stall, even though I'm executing from ITCM RAM?

My current work-around is to slow APB1 so much that the WWDG only needs servicing roughly once a second, and to do that I needed to slow AHB a long way as well. I don't like doing this but it seems to work (even if I leave my FLASH-writing code in FLASH).

One suspected bug I encountered is that the routine EE_VerifyPageFullyErased() seems to check from the specified starting address up to PAGE0_END_ADDRESS - so it cannot work when checking PAGE1.

Any comments?

2 REPLIES 2

Any read to FLASH during programming will stall the processor. This includes reads of (constant) data - are you sure the routine moved to ITCM RAM does not read constants from FLASH? (hint: examine disassembly or assembler listing; or step through in debugger observing the target addresses from which ldr read).

In F7, I am not sure if the processor+cache may perform significant amount of prefetch, which would run in parallel with execution from ITCM RAM for long enough to cause this sort of problems, but if you find no other culprit, it may be worth to try to go along this path too.

JW

Danish1
Lead III

The source-code around the fault (from stm32f7xx_hal_flash_ex.c) is as below. I have added the suffix _RAM to routines that are placed in ITCM RAM:

      /* Erase by sector by sector to be done*/
      for(index = pEraseInit->Sector; index < (pEraseInit->NbSectors + pEraseInit->Sector); index++)
      {
        FLASH_Erase_Sector_RAM(index, (uint8_t) pEraseInit->VoltageRange);
 
        /* Wait for last operation to be completed */
        status = FLASH_WaitForLastOperation_RAM((uint32_t)FLASH_TIMEOUT_VALUE);
        
        /* If the erase operation is completed, disable the SER Bit and SNB Bits */
        CLEAR_BIT(FLASH->CR, (FLASH_CR_SER | FLASH_CR_SNB)); 
 
        if(status != HAL_OK) 
        {
          /* In case of error, stop erase procedure and return the faulty sector*/
          *SectorError = index;
          break;
        }
      }

Single-stepping disassembly is (too small for me to see):

0690X000006Bv7qQAC.png

Or as a code-snippet without the addresses

    9B01        ldr r3, [sp, #4]
    689B        ldr r3, [r3, #8]
    9302        str r3, [sp, #8]
    E01E        b 0x0000010C
    9B01        ldr r3, [sp, #4]
    691B        ldr r3, [r3, #16]
    B2DB        uxtb r3, r3
    4619        mov r1, r3
    9802        ldr r0, [sp, #8]
    F000F830    bl 0x0000013C <FLASH_Erase_Sector_RAM>
    F24C3050    movw r0, #0xC350
    F000F886    bl 0x000001F0 <FLASH_WaitForLastOperation_RAM>
    4603        mov r3, r0
    F88D300F    strb.w r3, [sp, #15]
    4B12        ldr r3, =0x40023C00
    691B        ldr r3, [r3, #16]
    4A11        ldr r2, =0x40023C00
    F02303FA    bic r3, r3, #0xFA
    6113        str r3, [r2, #16]
    F89D300F    ldrb.w r3, [sp, #15]

If I execute by single-step the "9802 ldr r0, [sp, #8]" then I get the fault. So by implication we're getting enough speculative-execution of enough of "bl <FLASH_Erase_Sector_RAM>" to start the write. I've specified FLASH_VOLTAGE_RANGE_3 so there's quite a lot of code to execute in:

//void RUN_IN_RAM_SECTION FLASH_Erase_Sector_RAM(uint32_t Sector, uint8_t VoltageRange)
//{
    B086        sub sp, sp, #24
    9001        str r0, [sp, #4]
    460B        mov r3, r1
    F88D3003    strb.w r3, [sp, #3]
//--- stm32f7xx_hal_flash_ex.c -- 583 ------------------------
//uint32_t tmp_psize = 0;
    2300        movs r3, #0
    9305        str r3, [sp, #20]
//--- stm32f7xx_hal_flash_ex.c -- 585 ------------------------
///* Check the parameters */
//assert_param(IS_FLASH_SECTOR(Sector));
//assert_param(IS_VOLTAGERANGE(VoltageRange));
//if(VoltageRange == FLASH_VOLTAGE_RANGE_1)
    F89D3003    ldrb.w r3, [sp, #3]
    2B00        cmp r3, #0
    D102        bne 0x00000158
//--- stm32f7xx_hal_flash_ex.c -- 590 ------------------------
//{
//tmp_psize = FLASH_PSIZE_BYTE;
    2300        movs r3, #0
    9305        str r3, [sp, #20]
    E012        b 0x0000017E
//--- stm32f7xx_hal_flash_ex.c -- 592 ------------------------
//}
//else if(VoltageRange == FLASH_VOLTAGE_RANGE_2)
    F89D3003    ldrb.w r3, [sp, #3]
    2B01        cmp r3, #1
    D103        bne 0x00000168
//--- stm32f7xx_hal_flash_ex.c -- 594 ------------------------
//{
//tmp_psize = FLASH_PSIZE_HALF_WORD;
    F44F7380    mov.w r3, #0x100
    9305        str r3, [sp, #20]
    E00A        b 0x0000017E
//--- stm32f7xx_hal_flash_ex.c -- 596 ------------------------
//}
//else if(VoltageRange == FLASH_VOLTAGE_RANGE_3)
    F89D3003    ldrb.w r3, [sp, #3]
    2B02        cmp r3, #2
    D103        bne 0x00000178
//--- stm32f7xx_hal_flash_ex.c -- 598 ------------------------
//{
//tmp_psize = FLASH_PSIZE_WORD;
    F44F7300    mov.w r3, #0x200
    9305        str r3, [sp, #20]
    E002        b 0x0000017E
//--- stm32f7xx_hal_flash_ex.c -- 600 ------------------------
//}
//else
//{
//tmp_psize = FLASH_PSIZE_DOUBLE_WORD;
    F44F7340    mov.w r3, #0x300
    9305        str r3, [sp, #20]
//--- stm32f7xx_hal_flash_ex.c -- 604 ------------------------
//}
///* Need to add offset of 4 when sector higher than FLASH_SECTOR_11 */
//if(Sector > FLASH_SECTOR_11)
    9B01        ldr r3, [sp, #4]
    2B0B        cmp r3, #11
    D902        bls 0x0000018A
//--- stm32f7xx_hal_flash_ex.c -- 608 ------------------------
//{
//Sector += 4;
    9B01        ldr r3, [sp, #4]
    3304        adds r3, #4
    9301        str r3, [sp, #4]
//--- stm32f7xx_hal_flash_ex.c -- 610 ------------------------
//}
///* If the previous operation is completed, proceed to erase the sector */
//FLASH->CR &= CR_PSIZE_MASK;
    4B18        ldr r3, =0x40023C00
    691B        ldr r3, [r3, #16]
    4A17        ldr r2, =0x40023C00
    F4237340    bic r3, r3, #0x300
    6113        str r3, [r2, #16]
//--- stm32f7xx_hal_flash_ex.c -- 614 ------------------------
//FLASH->CR |= tmp_psize;
    4B15        ldr r3, =0x40023C00
    691A        ldr r2, [r3, #16]
    4914        ldr r1, =0x40023C00
    9B05        ldr r3, [sp, #20]
    4313        orrs r3, r2
    610B        str r3, [r1, #16]
//--- stm32f7xx_hal_flash_ex.c -- 615 ------------------------
//CLEAR_BIT(FLASH->CR, FLASH_CR_SNB);
    4B12        ldr r3, =0x40023C00
    691B        ldr r3, [r3, #16]
    4A11        ldr r2, =0x40023C00
    F02303F8    bic r3, r3, #0xF8
    6113        str r3, [r2, #16]
    23F8        movs r3, #0xF8
    9304        str r3, [sp, #16]
//--- cmsis_gcc.h -- 531 -------------------------------------
//{
//uint32_t result;
//#if (__CORTEX_M >= 0x03U) || (__CORTEX_SC >= 300U)
//__ASM volatile ("rbit %0, %1" : "=r" (result) : "r" (value) );
    9B04        ldr r3, [sp, #16]
    FA93F3A3    rbit r3 ,r3
    9303        str r3, [sp, #12]
//--- cmsis_gcc.h -- 544 -------------------------------------
//s--;
//}
//result <<= s; /* shift when v's highest bits are zero */
//#endif
//return(result);
    9B03        ldr r3, [sp, #12]
//--- stm32f7xx_hal_flash_ex.c -- 612 ------------------------
///* If the previous operation is completed, proceed to erase the sector */
//FLASH->CR &= CR_PSIZE_MASK;
//FLASH->CR |= tmp_psize;
//CLEAR_BIT(FLASH->CR, FLASH_CR_SNB);
//FLASH->CR |= FLASH_CR_SER | (Sector << POSITION_VAL(FLASH_CR_SNB));
    FAB3F383    clz r3, r3
    9A01        ldr r2, [sp, #4]
    FA02F303    lsl.w r3, r2, r3
    F0430202    orr r2, r3, #2
    4B08        ldr r3, =0x40023C00
    691B        ldr r3, [r3, #16]
    4907        ldr r1, =0x40023C00
    4313        orrs r3, r2
    610B        str r3, [r1, #16]
//--- stm32f7xx_hal_flash_ex.c -- 617 ------------------------
//FLASH->CR |= FLASH_CR_STRT;
    4B05        ldr r3, =0x40023C00
    691B        ldr r3, [r3, #16]
    4A04        ldr r2, =0x40023C00
    F4433380    orr r3, r3, #0x10000
    6113        str r3, [r2, #16]
//--- cmsis_gcc.h -- 429 -------------------------------------
//It completes when all explicit memory accesses before this instruction complete.
//*/
//__attribute__((always_inline)) __STATIC_INLINE void __DSB(void)
//{
//__ASM volatile ("dsb 0xF":::"memory");
    F3BF8F4F    dsb sy
//--- stm32f7xx_hal_flash_ex.c -- 618 ------------------------
///* Data synchronous Barrier (DSB) Just after the write operation
//This will force the CPU to respect the sequence of instruction (no optimization).*/
//__DSB();
//}
    BF00        nop
    B006        add sp, sp, #24
    4770        bx lr
    BF00        nop
    40023C00    .word 0x40023C00

So I'm not convinced of that amount of prefetch/speculative execution.

  • Danish