cancel
Showing results for 
Search instead for 
Did you mean: 

Embedded Flash memory in STM32F401xD

T B
Associate II

The STM32F401xD has 384Kbytes FLASH and the STM32F401xE has 512Kbytes FLASH.

Is there a mistake in the reference manual?

3.3 Embedded Flash memory in STM32F401xB/C and STM32F401xD/E

According to the manual STM32F401xD/E have the same number of sectors. I would expect that only STM32F401xE has an additional sector 7.

0693W00000LvwJ9QAJ.png

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

We are sorry that this was somewhat misleadingly expressed in RM0368.

Table 5 should be read as:

  • STM32F401xD has the Flash sectors 0...6, i.e. total=384KB
  • STM32F401xE has the Flash sectors 0...7, i.e. total=512KB

Does it answer our question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

We are sorry that this was somewhat misleadingly expressed in RM0368.

Table 5 should be read as:

  • STM32F401xD has the Flash sectors 0...6, i.e. total=384KB
  • STM32F401xE has the Flash sectors 0...7, i.e. total=512KB

Does it answer our question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.