‎2022-09-28 1:24 AM
Hi everyone; i followed the tutorial to get two output PWM signal with 10us of death time but i also tried to do a double complementary death time to have 4 signals with rispect death time but it doesn't work. In the main i add two mor command
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_3);
In this way i get two complementary pwm out put signal with death time on channel 2 e 2N but nothing on the other two channel 3 and 3N. This depend of the hardware of my board or i make some error in the setting?
‎2022-09-28 2:05 AM
maybe i found the issue: for channel_3 (also for channel 1) there is no option in Mode to select PWM mode. This mode is only avaiable on channel 2 where the code working
‎2022-09-28 5:24 AM
PWM mode with dead time :
‎2022-09-28 7:31 AM
Maybe you're just blocking the TIM1_CH1N/TIM1_CH3N pins with some other functionality?
JW
‎2022-09-28 7:57 AM
I forgot to select the PMW Mode for Channel_2 and now is working
‎2022-09-28 7:58 AM
sorry the pulse value