2022-02-15 12:12 AM
2022-02-16 03:51 AM
Hello @dost,
Chahinez.
2022-02-16 02:21 AM
Hello @dost,
As per the STM32L552xx datasheet, the Flash interface features are as follows:
And referring to the RM0438, the Flash memory has the following main features:
Please mark my answer as best by clicking on the "Select as Best" button if it fully answered your question. This will help other users find this solution faster.
Chahinez.
2022-02-16 02:38 AM
Hallo @ChahinezC ,
thank you for your answer, but just copying the datasheet and reference manual isn't helpful. It just says, that the capacity is up to 512 Kbytes and it can be organized in dual-bank mode with 2x256 Kbytes.
For the STM32L552CE with its flash size of 512 Kbytes it's all clear.
But what is with the STM32L552CC with a total flash size of just 256 Kbytes? Does it have just one bank with 1x256 Kbytes oder two with 2x128 Kbytes? There should be more information in the reference manual, the STM32L552CC variant isn't mentioned at all.
Best regards,
Markus
2022-02-16 03:51 AM
Hello @dost,
Chahinez.
2022-02-23 04:40 AM
Internal ticket number: 123359.
This is an internal tracking number and is not accessible or usable by customers.
Thank you.