cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32H743 have integrated crystal load capacitors?

BobaJFET
Associate II

I notice that on the NUCLEO-H753ZI board schematic and BOM, the load capacitors are not populated for X2. My thought is that these caps must exist elsewhere, either built into the crystal, or integrated into the STM32H743.. But I do not see any mention of integrated capacitors for either the microcontroller or the NX3215SA crystal datasheets. How can this work? 

NUCLEO-H753ZI - STM32 Nucleo-144 development board with STM32H753ZI MCU, supports Arduino, ST Zio and morpho connectivity - STMicroelectronics

BobaJFET_0-1733770911419.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

No, you'll need load caps. The 32 KHz used to be a DNF also, on a lot of the NUCLEO boards

h753zi_32khz.jpg

Pull the BoM from the product's "CAD Resources" tab/page

Check if X2 using a 6, 9 or 12pF crystal. Most of the ST parts used/expected 6-7pF crystals

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

No, you'll need load caps. The 32 KHz used to be a DNF also, on a lot of the NUCLEO boards

h753zi_32khz.jpg

Pull the BoM from the product's "CAD Resources" tab/page

Check if X2 using a 6, 9 or 12pF crystal. Most of the ST parts used/expected 6-7pF crystals

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
SofLit
ST Employee

Hello @BobaJFET ,

I think schematics is missing C71 and C72 capacitors as X2 is soldered. So either you solder X2, C71, C71 or you can unsolder all of them if the external crystal is not used.

There is no internal CL capacitors on the chip.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

Much appreciated.