2017-03-12 9:12 AM
Hi. I have an STM32F746 Discovery board purchased late last year from Digi-Key. It uses a STM32F746NG chip. I have not found any documentation anywhere that defines which revision of the Cortex M-7 core it uses. I am programing using FreeRTOS and its portability layer has a port.c function for the CM-7 core revision r0p1. I see the latest (but still dated 2015) ARMCortex-M7 Processor Technical Reference Manual is Revision r1p0 which presumably is later than revision r0p1.
How do I find out what revision the core is in any particular STM ARM chip?Thanks.
Solved! Go to Solution.
2017-03-13 3:29 AM
Hi,
As mentioned by Clive One, you may find more details in the
:2017-03-12 12:58 PM
I have a decoder for this and the FPU variant, but not near the system it is on
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0489d/Cihhbddh.html
SCB->CPUID <- check this register
DBGMCU->IDCODE
https://community.st.com/0D50X00009XkaRrSAJ
2017-03-12 12:59 PM
Check SCB->CPUID
printf('r%dp%d\n', ((SCB->CPUID >> 20) & 0x0F), (SCB->CPUID & 0x0F));
2017-03-12 5:04 PM
Clive, thanks for the info. on the SCB->CPUID register. It is documented, as I found out, in the PM0253 Cortex-M7 Programming manual. By the time I read your second post here I had already written a routine to recover the rnpn number.
And I discovered that it is r0p1 for the STM32F746NG chip as used in the STM746 Discovery kit. One of the links you gave above mentioned they thought that STM had only licensed the r0p1 core from ARM.
Thanks to all who have posted.
2017-03-12 5:30 PM
One of the threads went through a couple of edits, but the NUCLEO-F767 had the r1p0 part, the FPU-D and 2MB of FLASH
The FPU-S devices probably just going to be the r0p1 core, unless ST steps the part, and that would reflect in the errata documentation.
2017-03-13 3:29 AM
Hi,
As mentioned by Clive One, you may find more details in the
:2017-03-13 8:43 AM
Ok, but what are the plans moving forward? Is the core going to be updated in future releases of the F74xxx and F75xxx products?
2017-03-13 8:47 AM
Posted on March 13, 2017 at 15:47
Stuff with code tends to get locked in moderation for a while. These are the routines I built to do quick diagnostic checks
//****************************************************************************
void CORECheck(void) // sourcer32@gmail.com
{
uint32_t cpuid = SCB->CPUID;
uint32_t var, pat;
printf("CPUID %08X DEVID %03X REVID %04X\n", cpuid, DBGMCU->IDCODE & 0xFFF, (DBGMCU->IDCODE >> 16) & 0xFFFF);
pat = (cpuid & 0x0000000F);
var = (cpuid & 0x00F00000) >> 20;
if ((cpuid & 0xFF000000) == 0x41000000) // ARM
{
switch((cpuid & 0x0000FFF0) >> 4)
{
case 0xC20 : printf("Cortex M0 r%dp%d\n", var, pat); break;
case 0xC60 : printf("Cortex M0+ r%dp%d\n", var, pat); break;
case 0xC21 : printf("Cortex M1 r%dp%d\n", var, pat); break;
case 0xC23 : printf("Cortex M3 r%dp%d\n", var, pat); break;
case 0xC24 : printf("Cortex M4 r%dp%d\n", var, pat); break;
case 0xC27 : printf("Cortex M7 r%dp%d\n", var, pat); break;
default : printf("Unknown CORE\n");
}
}
else
printf("Unknown CORE IMPLEMENTER\n");
}
//****************************************************************************
// FPU Programmer Model
// http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0489b/Chdhfiah.html
void FPUCheck(void) // sourcer32@gmail.com
{
uint32_t mvfr0;
printf("%08X %08X %08X\n%08X %08X %08X\n",
*(volatile uint32_t *)0xE000EF34, // FPCCR 0xC0000000
*(volatile uint32_t *)0xE000EF38, // FPCAR
*(volatile uint32_t *)0xE000EF3C, // FPDSCR
*(volatile uint32_t *)0xE000EF40, // MVFR0 0x10110021 vs 0x10110221
*(volatile uint32_t *)0xE000EF44, // MVFR1 0x11000011 vs 0x12000011
*(volatile uint32_t *)0xE000EF48); // MVFR2 0x00000040
mvfr0 = *(volatile uint32_t *)0xE000EF40;
switch(mvfr0)
{
case 0x00000000 : puts("No FPU"); break;
case 0x10110021 : puts("FPU-S Single-precision only"); break;
case 0x10110221 : puts("FPU-D Single-precision and Double-precision"); break;
default : puts("Unknown FPU");
}
}
//****************************************************************************
Edited 5-Dec-2018, the forum transition totally snarled up the code formatting, reposting with clean/current code.
2017-03-14 3:23 AM
Hi Clive,
There is no plan for new device revision for F74xxx and F75xxx products.
So, there is no plan to embed a new core revision.
Thanks
Imen
2018-02-15 11:55 AM
The H743ZI has the Cortex-M7 r1p1 core
CPUID 411FC271 DEVID 450
Cortex M7 r1p1STM32H7xx
C0000018 2000B328 00000000
10110221 12000011 00000040FPU-D Single-precision and Double-precision