2014-02-24 7:42 AM
2014-03-08 2:15 AM
Thanks Francescato Diego and Clive.
I was pushed to work this way as the hardware is already designed and I have to just write firmware for it. Yes, I have no issue with the SD card speed as far as rest of the project requirement. I achieved 3Mb/s tested today. Yes I was thinking about NAND memory and compression algorithms before I started to attempt this project but cost was an issue as this (DCMI to SD) is a part of that project. Any how I have one more idea I'll try that. I'll try to capture odd and even fields I think interlacing is the word for it. I'll update that if I have done it like this.... Cheers.. :)2015-01-25 4:18 PM
@ali.babar
Did you manage to get any further with this high bandwidth DCMI > SDIO concept? I am looking to achieve similar (without external memory). It would be handy to know what type of throughput you managed to achieve?I am looking at splitting it up and receiving parts of the frame over multiple frames (as camera has function to repeat frames) if the throughput is not possible.