Question
STM32F205RCTb USB OTG FS :Is Pull up required on DP
Posted on January 25, 2015 at 18:13
We are using USB FS ( PA11 / PA12 ) in device mode. We have grounded ID pin i.e. PA 10 .We have not used any Pull up or pull down on DP and DM pin as described in eval board schematics STM32 20-21-45-46 G-EVAL USB_OTG_FS .
We received our actual application board with STM32F205RCTb, till now we were using Evaluation Board(STM3220G-EVAL). We used USB Device sample example(stm32cubef2) in FS mode on Eval Board, it worked fine. IDE used is IAR In our fabricated boards : When boot loader is there i.e without any firmware loaded board in Host PC. Now we are trying to port the eval kit code into our actual board(STM32F205RCTb), however the board is not detected as device in PC(Host). We modified target controller(STM32F205RC) and preprocessor(STM32F205XX) in project settings. Is there any external Pull up required on DP to detect the board as device in PC.