cancel
Showing results for 
Search instead for 
Did you mean: 

DMA UART with HAL remains busy bug new version

IK.2
Associate

I generated the code for the uart in dma mode in a cube. But the data does not go, and the HAL_UART_Transmit_DMA function returns HAL_BUSY.

I already found a solution to the problem, just publish it.

The cube generates code:

MX_USART2_UART_Init ();

MX_DMA_Init ();

At the same time, in the first line of the indicated ones, it writes to the DMA registers, but they are not clocked and therefore nothing is written. Adding a block before MX_USART2_UART_Init () helped;

In my example, a working initialization looks like this:

/ * Configure the system clock * /

SystemClock_Config ();

/ * USER CODE BEGIN SysInit * /

MX_DMA_Init (); // need for normal uart work

/ * USER CODE END SysInit * /

/ * Initialize all configured peripherals * /

MX_GPIO_Init ();

MX_LPUART1_UART_Init ();

MX_USART2_UART_Init ();

MX_DMA_Init ();

thank

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0