cancel
Showing results for 
Search instead for 
Did you mean: 

DMA and two or more U(S)ARTs

pawwodko
Associate II
Posted on October 03, 2013 at 09:50

Can I configure two usart's to use one DMA? In datasheet there is table called ''DMAx request mapping'' and for stm32f40/1/2/3 eg. UART4 uses

channel 4 for RX and TX DMA trigger on stream 2 and 4.

Can I configure stream 0 and 5 to use UART5 (also chanell 4) at the same time or this setting will collide with settings of UART4 DMA ?

#stm32-usart-dma
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User
Posted on October 03, 2013 at 10:26

Look at the DMA module as 8 independent DMA controllers, one per stream.

JW
pawwodko
Associate II
Posted on October 04, 2013 at 08:18

Triggering channels are also totally independent?

Posted on October 04, 2013 at 11:44

Each stream can be trigger by a single channel (8-to-1 mux)

The stream is the active DMA transaction, the channel is the source of the request.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..