2023-08-03 4:36 PM
Greetings,
I am writing here because I am out of solution for making the F401CC RTC use the reference clock detection feature to correct its timing. Everything in the RTC is working fine in my application, except for that feature. I use a STM32F401CCU6 (UQFN48 package) on a Black Pill board.
To verify whether the RTC is syncing off the external reference, I compare the RTC 1 Hz calibration output (pin PC13) to the 60 Hz (pin PB15) on an oscilloscope triggered by the 1 Hz. I cannot see any alignment effort whatsoever between the two signals. All I see is the frequency offset between the 32KHz resonator (LSE clock) and the 60 Hz reference, a slow drift of the 60 Hz signal on the screen. BTW, I use a lab-grade function generator to provide the 60 Hz (HP 33120A).
I use the STM32RTC library to get going, but then apply changes directly into the RTC registers to setup for, and enable the RTC reference clock detection, a feature not covered in the library. Here is the part of my Arduino code that deals with that feature (sorry for the French comments).
...
...
...
rtc.setClockSource(STM32RTC::LSE_CLOCK); // Selection du résonateur 32KHz comme source de l'horloge RTC
rtc.begin(); // initialisation de l'horloge RTC
// Input pin configuration for 50/60 Hz external reference
GPIOB->MODER &= 0x7FFFFFFF; // Configuration de la broche PB15 en entrée
GPIOB->PUPDR &= 0x3FFFFFFF; // Configuration de la broche PB15 sans pullup/pulldown
GPIOB->AFR[1] &= 0x0FFFFFFF; // Configuration de la broche PB15 sans fonction alternative
// RTC register unlock and transition into RTC Init mode
RTC->WPR = 0xCA; // Deverrouillage des registres du RTC
RTC->WPR = 0x53; // "
RTC->ISR |= RTC_ISR_INIT; // Entrer en mode Init
while (!((RTC->ISR) & RTC_ISR_INITF)); // Attendre que le mode Init soit confirmé
// Disabling of shift feature and coarse calibration
RTC->SHIFTR &= 0x7FFF8000;
RTC->CALIBR &= 0xFFFFF60; // Pas d'ajustement grossier du RTC
// Prescalers setting
RTC->PRER &= 0xFF808000; // Effacer les prescalers.
RTC->PRER |= 0x000000FF; // D'abord, PREDIV_S doit être 0x00FF pour un hotloge externe de 32.768 KHz.
RTC->PRER |= 0x007F0000; // Ensuite, PREDIV_A doit être 0x007F.
// Setup of 1 Hz calibration output and reference clock detection activation
RTC->CR &= 0xFF000000; // Envoyer la reference interne en sortie PC13.
RTC->CR |= RTC_CR_BYPSHAD; // Lire directement des registres du calendrier, pas des registres fantômes
RTC->CR |= RTC_CR_COE; // "
RTC->CR |= RTC_CR_COSEL; // Configurer fréquence de la reference en sortie à 1 Hz
RTC->CR |= RTC_CR_REFCKON; // Activer la detection de reference externe 50/60Hz
// Exit of Init mode
RTC->ISR &= !RTC_ISR_INIT; // Sortir du mode Init
while ((RTC->ISR) & RTC_ISR_INITF); // Attendre la sortie du mode Init
// RTC register lock
RTC->WPR = 0xFF; // Verrouillage des registres du RTC
...
...
...Here is what I have tried to debug:
Solved! Go to Solution.
2023-08-04 11:45 AM
You may want to have a look at https://community.st.com/t5/stm32-mcu-products/issue-with-the-rtc-ref-in-on-stm32f439nihx/td-p/62167
The point is, that you have to set PB15 as AF, i.e. 0b10. You use only &, which clears the uppermost bit in GPIOB_MODER which is already zero by default; while you are supposed to set it.
JW
2023-08-04 9:42 AM
I am afraid there's not much expertize here for the 50/60Hz calibration; myself included.
You can try to search this forum, I remember this being discussed in the past but I am afraid with no conclusion whatsoever.
Please note that this is a primarily user-driven forum with casual ST presence. You may want to contact ST directly, through FAE or the web support form.
JW
2023-08-04 11:45 AM
You may want to have a look at https://community.st.com/t5/stm32-mcu-products/issue-with-the-rtc-ref-in-on-stm32f439nihx/td-p/62167
The point is, that you have to set PB15 as AF, i.e. 0b10. You use only &, which clears the uppermost bit in GPIOB_MODER which is already zero by default; while you are supposed to set it.
JW
2023-08-04 1:55 PM
You got it, JW! "Properly" configuring the PB15 input as AF0 did it:
GPIOB->MODER &= 0x0FFFFFFF; // Configuration de la broche PB15 en AF0
GPIOB->MODER |= 0x80000000; // "
That RTC_REFIN signal is defined as an "Additional Function" in the pin list, not an "Alternate Function". This is where my confusion came from. Admittedly, elsewhere in the datasheet, it is written:
To use an I/O in a given configuration, proceed as follows:
• System function
Connect the I/O to AF0 and configure it depending on the function used:
– RTC_REFIN: this pin should be configured in Input floating mode
So Additional Function implies Alternate Function 0.
I thank you much! Have a good weekend.
Bert.