2019-11-26 10:40 PM
Hello,
i disable the interuppt after its execution is it allowed?
void EXTI4_IRQHandler(void)
{
// Clear interrupt
__HAL_GPIO_EXTI_CLEAR_IT(SYNC_UC_PIN);
// call function
function();// the function enables an other interrupt of the same priority
HAL_NVIC_DisableIRQ(EXTI4_IRQn);//disable the interrupt trigger SYNC_UC_PIN
}
after that i enable it after 200 millisecconds:
//activate flash interrupt
while (HAL_NVIC_GetPendingIRQ(EXTI4_IRQn))//clear interrupt pending bits
{
__HAL_GPIO_EXTI_CLEAR_IT(SYNC_UC_PIN);
HAL_NVIC_ClearPendingIRQ(EXTI4_IRQn);
}
2019-11-26 10:51 PM
Yes.
You will need an EnableIRQ() function to enable it, the ClearPendingIRQ() is something different.
JW
PS. Please change your username to a normal nick.
2019-11-26 11:21 PM
Hi changed the name.
Yes after deleting the pendig bit i enable it.
HAL_NVIC_EnableIRQ(EXTI4_IRQn); //enable interrupt for triggern
But i tryed to modify the interrupt Handler and i place the disable interrupt before the function()
then the sofware does not work properly.
void EXTI4_IRQHandler(void)
{
// Clear interrupt
__HAL_GPIO_EXTI_CLEAR_IT(SYNC_UC_PIN);
HAL_NVIC_DisableIRQ(EXTI4_IRQn);//disable the interrupt trigger SYNC_UC_PIN
// call function
function();// the function enables an other interrupt of the same priority
}
2019-11-26 11:59 PM
What do you mean by "does not work properly"?
The other interrupt of the same priority will not be called until you exit this interrupt.
JW
2019-11-27 12:33 AM
When i trigger the SYNC_UC_PIN in the seccond case, with the disabling interrupt at first place in handler.
Then the other interrupt enabling in the function does not occurs .
void function(void)
{
..
HAL_NVIC_EnableIRQ(ADC_IRQn);
..
}
The SYNC_UC_PIN triggers on its own again even if it is dissabled when an new signal SYNC_UC_PIN comes.
2019-11-27 1:16 AM
I don't understand.
Maybe prepare a minimal but complete compilable example exhibiting the problem.
JW
2019-11-27 2:14 AM
Hi,
If my system is ready i enable the interrupt EXTI4_IRQn . I trigger this interrupt EXTI4_IRQn in worst case every 300Hz and it comes through only when the system is ready, that means Enable HAL_NVIC_EnableIRQ(EXTI4_IRQn). As the interrupt happens in the irqhandler i disable it because my system will not be ready enymore and i start an analog digital converter mesurement ADC_IRQn. The ADC_IRQ is programmed as an watchdog and when the system reaches a state it triggers.
When i disable the EXTI4_IRQn before i call the function() then it seems that the ADC_IRQn does not mesure and the EXTI4_IRQn cause interrupt sometimes later on its on even if its dissabled.
thanks
2019-11-27 3:57 AM
Hi Can i Put the __DSB(); function after the disabling of EXTI4_IRQn in interupt handler ?