2018-01-03 1:22 AM
Hi,
I'm using a STM32L496VG, with an external LSE of 32768 Hz. I configure the RTC this way:
/* Enable Power Control clock */__HAL_RCC_PWR_CLK_ENABLE();/* Enable writing RTC back-up registers */HAL_PWR_EnableBkUpAccess();/* Configure RTC */RtcHandle.Instance = RTC;RtcHandle.Init.HourFormat = RTC_HOURFORMAT_24;RtcHandle.Init.AsynchPrediv = RTC_ASYNCH_PREDIV;RtcHandle.Init.SynchPrediv = RTC_SYNCH_PREDIV;RtcHandle.Init.OutPut = RTC_OUTPUT_DISABLE;RtcHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;RtcHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;HAL_RTC_Init(&RtcHandle);and:
/* Configure the RTC clock source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;RCC_OscInitStruct.LSEState = RCC_LSE_ON;HAL_RCC_OscConfig(&RCC_OscInitStruct);/* Select LSE as RTC clock source */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);/* Enable RTC Clock */
__HAL_RCC_RTC_ENABLE();In order to compensate the LSE drift, we output the RTC clock using HAL_RTCEx_SetCalibrationOutPut() function.
Using RTC_CALIBOUTPUT_1HZ we obtain 0.999951 Hz, which are 49 ppm drift, which is an expected value. But using RTC_CALIBOUTPUT_512HZ we obtain 508.022 Hz, which are 7769 ppm.
Also using an oscilloscope the output using RTC_CALIBOUTPUT_512HZ seems to be very unstable.
What's happening? Why there is such difference?
Thank you!
#rtc-calibration