cancel
Showing results for 
Search instead for 
Did you mean: 

Detect Memory leak check on stm32f7

phenom
Associate II

Hi,

I am working on stm32f779 eval kit.

How can I detect memory leaks on stm32?

Can anyone please suggest ways.

1 REPLY 1
Danish1
Lead III

You miss off some important information about your system.

What development software are you running? Some might have tools to help e.g. gcc has something called leaksanitizer.

Are you using c or c++? Is the leak with malloc/free or new/delete?

I think that you should avoid dynamic allocation where possible for embedded systems. But I understand that sometimes it’s unavoidable.

If you only have a few dynamic allocations then you could “instrument�? the calls - have wrappers around malloc/free that log the allocations. But that requires a relatively fast logging scheme.

Something I found useful was to be able to explore the heap and inspect any allocations that hadn’t been freed. In my case I reverse-engineered the heap code to add such a routine as full source was available. But your development system might provide that as standard.

Hope this helps,

Danish

PS: one further thought - do you have just the one thread (and no allocations in interrupts) or is your code multi-threaded with or without RTOS