2017-05-30 11:46 AM
Hello,
I am working with the STM32L486 chipset and we need to generate an exact 38400Hz timer. Currently we have a 5MHz or 25MHz external clock coming in but the PLL clock tree does not seem to favor getting the exact 38400Hz rate for a timer. Is it possible with the above external clock rates? or if not, any suggestions to get this, including a different rate for external clock source?
Thanks,
ED
Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2017-05-30 12:32 PM
At 12 MHz input clock you can run CPU at 24, 48 or 72 MHz
I believe an input of 4, 8 MHz would also offer these. An input of 24 MHz would provide for multiple additional options ranging from 19.2 thru 76.8 MHz
2017-05-30 12:32 PM
At 12 MHz input clock you can run CPU at 24, 48 or 72 MHz
I believe an input of 4, 8 MHz would also offer these. An input of 24 MHz would provide for multiple additional options ranging from 19.2 thru 76.8 MHz
2017-05-30 4:33 PM
Thanks Clive One! I found a crystal at 19.2MHz available that would also do the job.
2017-07-10 12:10 PM
Hi Clive One, for my own exercise, I revisited this thread to play around with the numbers in Cube's Clock Configuration and I couldn't seem to get the 24MHz input crystal to output 19.2MHz or 76.8MHz as you stated here. Can you elaborate on how to get to, say the 19.2MHz from a 24MHz input, as an example? Sorry to bring this up again!
2017-07-10 12:35 PM
I don't use Cube, I'm a mechanic, the fitter threw out these values
freq=24.0000 MHz
cpu= 19.2000, pll_m= 5, pll_n= 16, pll_p=4, pllcomp=4.800000
cpu= 19.2000, pll_m= 5, pll_n= 24, pll_p=6, pllcomp=4.800000 cpu= 19.2000, pll_m= 5, pll_n= 32, pll_p=8, pllcomp=4.800000 cpu= 76.8000, pll_m= 5, pll_n= 64, pll_p=4, pllcomp=4.8000002017-07-10 1:03 PM
Maybe I am missing something here but not sure if your fitter adheres to the clock tree specified by ST for a particular part, as shown below. How are the pll_m, pll_n, pll_p and pll_comp translating to the PLLMul, PLLDiv, AHB prescaler and APB1 prescaler, etc.?
2017-07-10 1:21 PM
Look at the RCC tree in RM.
M is the PLL prescaler. N is the multiplier - for some reason ST omitted that from the 'L4 RM picture; look into the same picture e.g. in RM0090. P is the postscaler - in the L4 that particular postscaler is used for a different purpose and R is used instead for SYSCLK output, again look into RM0090 for the 'original'.
pll_comp obviously is the PLL input frequency; you have to check that (and the PLL output freq too) against the PLL range given for particular chip in DS.
JW
2017-07-10 1:31 PM
The AHB/APB stuff is irrelevant, I went from the Reference Manual, and Data Sheet values for the VCO frequencies, and PLL comparison frequencies
Look at what Cube spits out for
HAL_RCC_OscConfig() boiler plate, and tune manually.
&sharpifdef USE_STM32L4XX_NUCLEO
/** * @brief System Clock Configuration * The system Clock is configured as follow : * System Clock source = PLL (MSI) * SYSCLK(Hz) = 80000000 * HCLK(Hz) = 80000000 * AHB Prescaler = 1 * APB1 Prescaler = 1 * APB2 Prescaler = 1 * MSI Frequency(Hz) = 4000000 * PLL_M = 1 * PLL_N = 40 * PLL_R = 2 * PLL_P = 7 * PLL_Q = 4 * Flash Latency(WS) = 4 * @param None * @retval None */void SystemClock_Config(void){ RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_OscInitTypeDef RCC_OscInitStruct = {0};/* MSI is enabled after System reset, activate PLL with MSI as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 40; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLP = 7; RCC_OscInitStruct.PLL.PLLQ = 4; HAL_RCC_OscConfig(&RCC_OscInitStruct);/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
clocks dividers */ RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4);}&sharpendif2017-07-10 1:38 PM
2017-07-10 1:44 PM
Well pll_comp is my computation for the comparison frequency (needs to be in range 4-16 MHz), there's not really a 'multiplier' it divides down the VCO frequency so that VCO / PLL_N == HSE / PLL_M, and pumps the VCO frequency up/down a tad to tune it.