cancel
Showing results for 
Search instead for 
Did you mean: 

debug when using visual com port

FMaup.1
Associate II

Hi,

My application will use intensively use Virtual Com Port to exchange datas from my board to the PC. I would like to make sure that debugging through STLink is still possible as i will be exchanging datas. Does St Link use the same USB port for debug and application ?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

You can use the VCP and debug at the same time. They're on the same physical USB port, but it's a composite device. The ST-Link and serial port act as separate devices.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

You can use the VCP and debug at the same time. They're on the same physical USB port, but it's a composite device. The ST-Link and serial port act as separate devices.

If you feel a post has answered your question, please click "Accept as Solution".
FMaup.1
Associate II

Ok thanks a lot