cancel
Showing results for 
Search instead for 
Did you mean: 

Custom usb

RJ1
Associate

Hi Team,

 

I'm using STM32H743 series controller.

I want to implement USB Base class on STM32H743. Unfortunately CubeMX will not support it.

Any example code which works on Base class- 00h, Sub class -00h and protocol -00h

2 REPLIES 2
Pavel A.
Evangelist III

Class 00h, sub class 00h, protocol 00h in the device descriptor means that the actual class/subclass/protocol are defined in the Interface descriptor, or (more likely) the device is composite and has several functions, with their  own descriptors. ST USB library has "composite builder" for creating composite devices, and USBX has support for composite devices.

Note: if by custom you mean the vendor specific class, it is not 00/00/00. Interface (USB function) with Class 00h, sub class 00h, protocol 00h is not valid.

 

 

FBL
ST Employee

Hi @RJ1 

You can get information from interface descriptors after it has been enumerated by host. But there is no example dedicated to base class.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!