2017-10-23 07:11 PM
Running latest 4.1 STM32CubeMx on both *buntu and Windows 7 and the generated stm32f4xx_hal_msp.c is totally different. The HAL libraries in both cases areSTM32Cube_FW_F4_V1.0.
With the Linux version, the following functions are missing:
which results (not surprisingly) a totally useless build.
This needs to be fixed urgently as I only have part-time access to a single windows machine to create the code if I change any pinouts etc.
Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-03-16 09:09 AM
I'm toying with the idea of making my own CubeMX for the Nucleo I have...
I'm oscillating between Processing (a fast mode in getting a nice graphical interface which I need for the clock setup), Lazarus+FreePascal (easy file manipulation, easy string manipulation and RAD) and Qt with C++...
It will generate for Makefile projects with LL drivers. Another option (and a strong temptation) is to make it generate for SPL.
2018-04-03 06:27 PM
Over 5 months in and still not even an acknowledgement of the problem.
Does anyone know of a way of escalating the issue with ST to at least get some confirmation that I'm not the only one with this issue?
This continues to impact my development and will now start to influence my choices of WIFI, BlueTooth, Accelerometer and NFC devices (currently
SPWF01, SPBTLE-RF, LSM6DSL,
CR95HF) if I can't get reliable product support.
2018-04-04 03:30 AM
Hello,
I will raise you request to the appropriate team for investigation.
Sorry for the inconvenience it may bring.
Best Regards,
Imen
2018-04-25 04:51 AM
Hi Frackers,
Thanks for your feedback and s
orry for late response.
I confirm the bug. The issue will be fixed in the next CubeMX release.
Please feel free to contact me for further details.
Best regards,
Mohamed
2018-05-13 11:21 PM
Just updated to 4.25.1 and it STILL doesn't work.
2018-05-14 02:31 AM
Hi
Gilks.Robin
,This issue will be fixed for the next release CubeMX 4.26 .Sorry for such inconvenience.
Best regards,
Mohamed.