cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.15.0 Bug Report

megaboy2k
Associate II
Posted on May 29, 2016 at 20:02

When some output configured as an alternative function, the only option available is ''Alternative Function Push Pull'' but according to Ref manual (e.g. for stm32f405) the Open Drain for alternative function is also possible and was required in my application.

11 REPLIES 11
megaboy2k
Associate II
Posted on June 02, 2016 at 18:26

Hannibal, you said that open-drain will not work in full-duplex configuration.

But why it really works in real hardware if I change GPIO_MODE_AF_PP to GPIO_MODE_AF_OD manually?

Also, where is in Ref manual (RM0090) mentioned that OD is not available in full-duplex mode?

Radosław
Senior II
Posted on June 02, 2016 at 19:45

bullshit, not true, etc.......

Standard (FULL DUPLEX) UART can work very vell with opendrain....