cancel
Showing results for 
Search instead for 
Did you mean: 

Cube IDE latest update Bug

msalem88
Associate II

There is a bug in the new cube ide version in the lwip vonfiguration for the STM32F7

 

LWIP_RAM_HEAP_POINTER (RAM Heap Pointer) 0x30004000

There is no such RAM location in the STM32F7. the correct value should be zero but better u guys check it.

 

by the way this option was not there for the F7 LWIP Key options settings in the previous cube ide version.

 

6 REPLIES 6
SofLit
ST Employee

Hello @msalem88 and welcome to the community,

CubeMx or CubeIDE? and which version?

How you did you reproduce the issue?

Do you have a project you can share?

Thanks.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
msalem88
Associate II

Hi

cube ide.

create project with f746 dk and you will get it. 

 

Sorry i can not share my project

 

We cannot help you if you don't have more details

You can share your project by sending it in private for analysis if you don't want to share it in public. 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I dont need to send any thing, i just createrd new project using STM3F746 DK and i found the problem again in clean project. its up to u to fix it or not!!.

Maybe the problem in the new Firmware package of the F7 not in the cube ide it self. 

i guess i am the one who is helping you here not you helping me!!

zxu
Associate

New since 6.13 in `lwipopts.h`:

/*----- Default Value for F7/H7 devices: 0x30044000 -----*/
#define LWIP_RAM_HEAP_POINTER 0x30004000

 

First I don't know why the value in the comment doesn't match with the actual value, second with these two extra lines generated, it breaks my program as in `MX_LWIP_INIT()` would not return. I guess OP isn't wrong.

I wrote it worng, default value for F7 /H7, the funny thing is no such location in the internal RAM for F7 and thats why it break with u same as with me.