2024-12-03 05:47 AM
There is a bug in the new cube ide version in the lwip vonfiguration for the STM32F7
LWIP_RAM_HEAP_POINTER (RAM Heap Pointer) 0x30004000
There is no such RAM location in the STM32F7. the correct value should be zero but better u guys check it.
by the way this option was not there for the F7 LWIP Key options settings in the previous cube ide version.
2024-12-03 06:19 AM - edited 2024-12-03 06:20 AM
Hello @msalem88 and welcome to the community,
CubeMx or CubeIDE? and which version?
How you did you reproduce the issue?
Do you have a project you can share?
Thanks.
2024-12-03 10:52 AM
Hi
cube ide.
create project with f746 dk and you will get it.
Sorry i can not share my project
2024-12-03 11:36 AM
We cannot help you if you don't have more details
You can share your project by sending it in private for analysis if you don't want to share it in public.
2024-12-03 03:46 PM
I dont need to send any thing, i just createrd new project using STM3F746 DK and i found the problem again in clean project. its up to u to fix it or not!!.
Maybe the problem in the new Firmware package of the F7 not in the cube ide it self.
i guess i am the one who is helping you here not you helping me!!