cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 MCU model shortlisting for Making RC remote

Palnerve
Visitor

Hi everyone,

  1. which type of stm32 microcontroller is best fit for following operations
  2. for building rc remote of 8 channel and more
  3. low cost
  4. low power consumption
  5. high-speed rf communication and easy integrate with RF chip using SPI port
  6. easy to design and develop
  7. 10-bit ADC
  8. low voltage
  9. display interference
  10. RTC
1 REPLY 1
STTwo-32
ST Employee

Hello @Palnerve and welcome to the ST Community.

I suggest you use the ST-MCU-FINDER-PC - STM32 and STM8 product finder for desktops - STMicroelectronics standalone or the STM32CubeMX integrated version:

STTwo32_0-1751894826464.png

Using the filters, you can select the MCU you are looking for according to the filters you select.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.