2023-09-25 12:17 AM
Hi,
I am working with STM32G491RE in my project. I have to transmit data through UART and I need to calculate CRC for that data.
in my application:
txdata[0] = 0x78;
txdata[1] = 0x04;
txdata[2] = 0x11;
txdata[3] = 0x01;
I have to calculate CRC16 for txdata[1] to txdata[3] and place it in txdata[4]& txdata[5].
1.I configured CRC parameters:
hcrc.Instance = CRC;
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
if (HAL_CRC_Init(&hcrc) != HAL_OK)
{
Error_Handler();
}
2. I am using following function to calculate CRC
HAL_CRC_Calculate(&hcrc, (uint8_t *)txdata[1] ,3);
is it correct way to do or need to change anything.
Can anyone suggest.
Thanks
Solved! Go to Solution.
2023-09-25 6:26 AM
In additional to @Tesla DeLorean 's comments:
> HAL_CRC_Calculate(&hcrc, (uint8_t *)txdata[1] ,3);
You are missing a & sign. It should be this:
HAL_CRC_Calculate(&hcrc, (uint8_t *)&txdata[1], 3);
2023-09-25 12:24 AM
2023-09-25 1:45 AM - edited 2023-09-25 2:49 AM
Hello @sireevenkat1,
HAL_CRC_Calculate() is used to compute the 7, 8, 16 or 32-bit CRC value of an 8, 16 or 32-bit data buffer independently of the previous CRC value. However, HAL_CRC_Accumulate() is being used depending on the combination of the previous CRC value and the new one in order to chain a CRC calculation. For further details check Using the CRC peripheral on STM32 microcontrollers - Application note.
I hope this help!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-25 1:47 AM
Hi @Issamos,
Thanks for the reply,
It will be helpful but my input data differs every time based on the other peripheral output.
If I use below api
HAL_CRC_Accumulate(&hcrc, (uint32_t *)&CRC16_DATA8_CHECK, BUFFER_SIZE);
Is it possible to calculate CRC16 for txdata[1] to txdata[3] leaving txdata[0].
Thanks
2023-09-25 2:29 AM
You haven't defined the width of the polynomial, or it's value.
What would be helpful would be to cite what the receiving device is, and then a couple of known good test parameters to confirm its is working properly. There's a lot of critical parameters as they are very sensitive to bit ordering and sequencing.
2023-09-25 6:26 AM
In additional to @Tesla DeLorean 's comments:
> HAL_CRC_Calculate(&hcrc, (uint8_t *)txdata[1] ,3);
You are missing a & sign. It should be this:
HAL_CRC_Calculate(&hcrc, (uint8_t *)&txdata[1], 3);
2023-10-12 5:28 AM - edited 2023-10-12 5:31 AM
Hi @Tesla DeLorean, @TDK
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
Is above statement don't make polynomial enable? Do I need to give value separately?
is below code correct way to do?
CRC_HandleTypeDef hcrc;
MX_CRC_Init();
static void MX_CRC_Init(void)
{
/* USER CODE BEGIN CRC_Init 0 */
/* USER CODE END CRC_Init 0 */
/* USER CODE BEGIN CRC_Init 1 */
/* USER CODE END CRC_Init 1 */
hcrc.Instance = CRC;
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
if (HAL_CRC_Init(&hcrc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CRC_Init 2 */
/* USER CODE END CRC_Init 2 */
}
void function()
{
txdata[0] = 0x13;
txdata[1] = 0x04;
txdata[2] = 0x15;
txdata[3] = ACK;
// compute CRC to place into last 2 bytes
uint16_t calculatedCRC = HAL_CRC_Calculate(&hcrc,(uint32_t *)&txdata[1], 3);
txdata[4] = calculatedCRC & 0xFF; //low CRC byte
txdata[5] = (calculatedCRC >> 8& 0xFF; //high CRC byte
txdata[6] = 0x05;
HAL_UART_Transmit(&huart5, txdata,7, HAL_MAX_DELAY);
}
Thanks
2023-10-12 5:37 AM
@Tesla DeLoreansaid above:
> What would be helpful would be to cite what the receiving device is, and then a couple of known good test parameters to confirm its is working properly. There's a lot of critical parameters as they are very sensitive to bit ordering and sequencing.
JW
2023-10-12 5:57 AM
So it's using the default 32-bit polynomial?
If you're using you own protocol it would be sufficiently that both ends process the data consistently and generate the same check bytes for the same data.
2023-10-12 10:18 PM
Hi @Tesla DeLorean,
1.So it's using the default 32-bit polynomial?-------I think so, not sure.
I am using STM32G4 series .As per CRC application note below tables says polynomial coefficient is programmable. Based on what basis do I need to select polynomial coefficient can you suggest.
I saw some posts in forum they are using below polynomial. Can you suggest how do select value for polynomial?
1.#define MODBUS_CRC_POLY 0x8005
2.#define MODBUS_CRC_POLY 0xA001
If I define my polynomial below configuration are sufficient?
hcrc.Init.GeneratingPolynomial = MODBUS_CRC_POLY; hcrc.Init.CRCLength = CRC_POLYLENGTH_16B; hcrc.Init.InitValue = 0xFFFF2.
3.My application is to send the data of sensors and status of some sensors to other module using UART. That module receives the data and send it to cloud.
Thanks