CORDIC Phases results largely differs from q1.31 to q1.15
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-01-09 7:19 AM - edited 2025-01-09 7:26 AM
Hello everyone !
I've recently hit a snag in a motor FOC project of mine: the CORDIC unit on a STM32G431xB doesn't give out similar q1.15 results when the input are 32 and 16 bits.
In the current setup, both sine an cosine coefficient are pre-stored as q1.15 values in two separate sensor input buffers (from hall resolvers).
In order to simulate actual q1.31 value, I simply left-shift the buffered q1.15 values by 16 upon use, and tolerates the LSB loss for the purposes of the tests.
Here's an excerpt of the test method :
[main loop]
float *pResA = resultsA, *pResB = resultsB; // For the purpose of the test, our q1.15 results will be converted to degrees as f32 values.
cnt = NB_ANGLE_SAMPLES;
CordicUnit::clearError();
while (cnt-- && !CordicUnit::hasError()) {
// Input sin/cos coeffs' are stored in q1.15 buffers, addressed through *pSin and *pCos.
// Both functions returns q1.15 results
*pResA++ = 180.0f + 180.0f * ((float)CordicUnit::atan2_i31_o15(int32_t(*pSin) << 16, (int32_t)(*pCos) << 16) / 32767); // fed truncated Q1.31 values.
*pResB++ = 180.0f + 180.0f * ((float)CordicUnit::atan2_i15_o15(*pSin, *pCos) / 32767); // fed the actual Q1.15 values.
pSin++;
pCos++;
}
[/main loop]
One would expect resultA and resultB contents to vary only by a few percents, however, that's not the case :
results from atan2_i31_o15
results from atan2_i31_o15
results from atan2_i15_o15
Wut ?
Here are the declarations & definitions of both, bare-metal CordicUnit::atan2xxxxx functions :
[declarations]
enum CordicFunction_e : uint32_t{
CORDIC_ATAN2_I31_O15 = (CORDIC_CSR_RESSIZE | CORDIC_NBWRITE_2 | (4 << CORDIC_CSR_PRECISION_Pos) | (2 << CORDIC_CSR_FUNC_Pos)),
CORDIC_ATAN2_I15_O15 = (CORDIC_CSR_ARGSIZE | CORDIC_CSR_RESSIZE | (4 << CORDIC_CSR_PRECISION_Pos) | (2 << CORDIC_CSR_FUNC_Pos)),
};
[/declarations]
[definitions]
int16_t CordicUnit::atan2_i31_o15(int32_t y, int32_t x)
{
if (_completedLast == false)
return 0;
CORDIC->CSR = CordicFunction_e::CORDIC_ATAN2_I31_O15;
CORDIC->WDATA = (uint32_t)x;
CORDIC->WDATA = (uint32_t)y;
_completedLast = false;
uint32_t start = micros(); // timeout timestamp
// Wait for completion, with some ample timeout (500µs)
while ((CORDIC->CSR & CORDIC_CSR_RRDY) == 0 && ((micros() - start) < 500))
asm(" nop");
// Timed out ?
if ((CORDIC->CSR & CORDIC_CSR_RRDY) == 0) {
_cordicHasErrors = true;
return 0;
}
_completedLast = true;
return (CORDIC->RDATA & 0xFFFFU); // discards the MSW and its modulus result
}
int16_t CordicUnit::atan2_i15_o15(int16_t y, int16_t x)
{
if (_completedLast == false)
return 0;
CORDIC->CSR = CordicFunction_e::CORDIC_ATAN2_I15_O15;
CORDIC->WDATA = (((uint32_t)y) << 16) | (uint32_t)x;
_completedLast = false;
uint32_t start = micros(); // timeout timestamp
// Wait for completion, with some ample timeout (500µs)
while ((CORDIC->CSR & CORDIC_CSR_RRDY) == 0 && ((micros() - start) < 500))
asm(" nop");
// Timed out ?
if ((CORDIC->CSR & CORDIC_CSR_RRDY) == 0) {
_cordicHasErrors = true;
return 0;
}
_completedLast = true;
return (CORDIC->RDATA & 0xFFFFU); // discards the MSW and its modulus result
}
[/definitions]
I'm quite at a loss here.
Using either q1.15 or q1.31 inputs isn't a costly time issue, but I cannot fathom why the results differ so much.
Any idea ?
Labels:
- Labels:
-
CORDIC
-
STM32G4 Series
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-02-25 7:27 PM
Nothing ? Was my exposé too long ? :confounded_face:
Well, having no response at all, and the CORDIC phase calculations still returning gibberish
I had to implement the CORDIC atan2 on the sensor side ( hosted by a measly CH32V003, but it manages to push out samples at 25Ksps, so I'm not complaining -yet- )
Here's the function code, for those interested : its crude, unoptimized, but gets the job done :
/** @brief Returns the angle of a cartesian coordinate relative to zero, expressed in the range [-1.0; 1.0]
* @PAram y,x Q15 signed numbers representing the sine and cosine components of the angle to be returned. */
*/
int16_t cordic_atan2_q15(int16_t y, int16_t x)
{
// Handle special cases where x or y is zero
if (x == 0 && y == 0) {
return 0;
}
if (x == 0) {
return (y > 0) ? 16384 : -16384; // π/2 or -π/2 in scaled Q15
}
if (y == 0) {
return (x > 0) ? 0 : 32767; // 0 or π (clamped to 32767)
}
// Determine the quadrant and take absolute values of x and y
int quadrant;
int16_t abs_x = abs(x);
int16_t abs_y = abs(y);
if (x > 0 && y > 0) {
quadrant = 0;
} else if (x < 0 && y > 0) {
quadrant = 1;
} else if (x < 0 && y < 0) {
quadrant = 2;
} else {
quadrant = 3;
}
// CORDIC algorithm in vectoring mode
int32_t x32 = (int32_t)abs_x;
int32_t y32 = (int32_t)abs_y;
int32_t z = 0;
// Precomputed atan_table in scaled Q15 (atan(2^-i)/π * 32768), rounded to nearest integer
static const int16_t atan_table[] = { 8192, 4836, 2555, 1297, 650, 326, 163, 81, 41, 20, 10, 5, 3, 1 };
const int num_iterations = sizeof(atan_table) / sizeof(atan_table[0]);
for (int i = 0; i < num_iterations; ++i) {
int32_t x_shifted = x32 >> i;
int32_t y_shifted = y32 >> i;
if (y32 >= 0) {
x32 += y_shifted;
y32 -= x_shifted;
z += atan_table[i];
} else {
x32 -= y_shifted;
y32 += x_shifted;
z -= atan_table[i];
}
}
// Adjust the angle based on the original quadrant
int32_t adjusted_angle;
switch (quadrant) {
case 0:
adjusted_angle = z;
break;
case 1:
adjusted_angle = 32768L - z;
break;
case 2:
adjusted_angle = z - 32768L;
break;
case 3:
adjusted_angle = -z;
break;
default:
adjusted_angle = 0;
break;
}
// Clamp the result to the valid Q15 range [-32768, 32767]
if (adjusted_angle > 32767) {
adjusted_angle = 32767;
} else if (adjusted_angle < -32768) {
adjusted_angle = -32768;
}
return (int16_t)adjusted_angle;
}
View more
Hope it helps. Never got the CORDIC coprocessor to work correctly anyway. :sad_but_relieved_face: