2020-06-16 06:54 AM
I created a project using the CubeMX software, as the basis for a music playing device.
I then used the SD disk io dma rtos driver from the wav player/recorder as the cube generated code is broken.
Can I put a project on github using the above code?
I've left the copyright agreements in place, but perhaps modified header references in places. Can anyone (perhaps an ST rep) provide guidance here?