cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446RET7 custom board flashing issue with SWD connector

TH.16.336
Associate III

Hello All,

We have an custom board using stm32f446re controller which has 6 PIN SWD JTAG connector.

We are using NUCLEO-F446RE kit as debugger to flash the custom board as explained in "6.2.4 Using ST-LINK/V2-1 to program and debug an external STM32 application" from below link,

https://www.st.com/content/ccc/resource/technical/document/user_manual/98/2e/fa/4b/e0/82/43/b7/DM00105823.pdf/files/DM00105823.pdf/jcr:content/translations/en.DM00105823.pdf

Removed CN2 jumpers

Connected CN4 SWD pins of NUCLEO-F446RE to custom SWD connector as appropriate signals.

But we are not flash or debug as we are getting below error in System workbench for STM32 IDE,

Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 480 kHz

adapter_nsrst_delay: 100

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 480 kHz

Info : STLINK v2 JTAG v31 API v2 SWIM v7 VID 0x0483 PID 0x3748

Info : using stlink api v2

Info : Target voltage: 3.223483

Info : Stlink adapter speed set to 480 kHz

Info : STM32F446RETx.cpu: hardware has 6 breakpoints, 4 watchpoints

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Error: timed out while waiting for target halted

TARGET: STM32F446RETx.cpu - Not halted

in procedure 'reset' 

in procedure 'ocd_bouncer'

Info : device id = 0x10006421

Warn : STM32 flash size failed, probe inaccurate - assuming 512k flash

Info : flash size = 512kbytes

Error: Target not halted

Error: failed erasing sectors 0 to 0

Error: flash_erase returned -304

Cross verified the FLASH SIZE and it's 512KB.

Can someone help here to understand the issue?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

Use a short cable for the interconnection, max. 15cm.

JW